2009-04-20  Rene Schipp von Branitz Nielsen <rbn@vitesse.com>

	* src/am29xxxxx.c: Added set of parentheses around macro
	parameters used in multiplications. Fixes 16as8 bug.

2008-12-19  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/flash_am29xxxxx_v2.cdl: Doh, fix doc link properly.

2008-11-20  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/flash_am29xxxxx_v2.cdl: Fix doc link.

2008-09-24  Bart Veer  <bartv@ecoscentric.com>

	* src/am29xxxxx_aux.c (am29_hw_program): fix handling of parallel
	chips. Get the debug diagnostics to build cleanly.

2008-05-13  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/am29xxxxx_aux.c (am29_hw_query): Allow devices to return
	device IDs of larger than a byte.

2007-07-08  Bart Veer  <bartv@ecoscentric.com>

	* src/am29xxxxx.c, src/am29xxxxx_aux.c: add 2ram entry and exit
	hooks to give HALs some extra control over the low-level flash
	operations.

2007-06-21  Bart Veer  <bartv@ecoscentric.com>

	* src/am29xxxxx_aux.c: issue a memory barrier after every command
	that gets sent to the flash, to avoid problems with pipelines that
	mess about with write ordering.

2007-05-31  Bart Veer  <bartv@ecoscentric.com>

	* src/am29xxxxx.c: skip data cache manipulation on architectures
	which do not have a data cache.

2007-05-29  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/flash_am29xxxxx_v2.cdl
	(CYGHWR_DEVS_FLASH_AMD_AM29XXXXX_V2_RESET_NEEDS_RESUME): New option.
	Allow Flash devices to indicate that they should be sent a "resume"
	command on startup.
	* src/am29xxxxx_aux.c (am29_hw_force_all_suspended_resume): New
	function to implement above CDL.
	(cyg_am29xxxxx_init_check_dev): Call the new function.
	(cyg_am29xxxxx_init_cfi): Ditto.
	(am29_hw_cfi): manufacturer_id and vendor private areas need only
	lowest byte taken, to handle multiple parallel devices.

2007-03-29  Bart Veer  <bartv@ecoscentric.com>

	* src/am29xxxxx_aux.c (am29_hw_erase): use DQ7 to detect
	termination instead of DQ6. This avoids hardware problems where
	the toggling of DQ6 is not detected.

	* cdl/flash_am29xxxxx_v2.cdl: increate the default erase burst
	duration a bit since the erase inner loop should now take fewer
	cycles, and one uncached memory access has been eliminated.

2007-03-05  Nick Garnett  <nickg@ecoscentric.com>

	* src/am29xxxxx_aux.c (am29_hw_cfi): Added missing AM29_SWAP() to
	fetch of offset of vendor specific data.

2006-10-10  Bart Veer  <bartv@ecoscentric.com>

	* src/am29xxxxx_aux.c (cyg_am29xxxxx_erase): fix builds which have
	ERASE_SUSPEND functionality disabled.

2006-09-27  Nick Garnett  <nickg@ecoscentric.com>

	* src/am29xxxxx_aux.c (am29_hw_cfi): Added generic code to deal
	with flash parts that may specify their erase regions in reverse
	order to reality. Removed older code that was too specific to
	particular devices.
	A few changes to the diagnostics in various places.

	* cdl/flash_am29xxxxx_v2.cdl: Replaced
	CYGHWR_DEVS_FLASH_AMD_AM29XXXXX_V2_AT49_CFI with
	CYGHWR_DEVS_FLASH_AMD_AM29XXXXX_V2_CFI_BOGOSITY. This option
	performs much the same purpose, but is generic to many more flash
	parts.

2006-08-31  Nick Garnett  <nickg@ecoscentric.com>

	* src/am29xxxxx_aux.c: Added support for ST flash parts which have
	similar, but not identical, peculiarities in their CFI data to the
	Atmel parts supported earlier.

2006-08-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/am29xxxxx.c: Provide a default HAL_MEMORY_BARRIER()
	define if the HAL hasn't provided one.
	* src/am29xxxxx_aux.c: Use HAL_MEMORY_BARRIER() any time the
	flash is reset back to read array mode. Some processors
	need to have their write buffers flushed.

2006-06-29  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/flash_am29xxxxx_v2.cdl:
	* src/am29xxxxx_aux.c:
	Added configurable delay between each word during
	programming. Some targets seem to need this.
	Also added some simple diagnostics.

2006-05-15  John Dallaway  <jld@ecoscentric.com>

	* doc/am29xxxxx.sgml: Fix missing </refentry> tag.
	* cdl/flash_am29xxxx_v2.cdl: Reference package documentation.

2005-09-26  Bart Veer  <bartv@ecoscentric.com>

	* src/am29xxxxx.c, src/am29xxxxx_aux.c: add AM29_SWAP() support for
	platforms where the bus connection is wired up strangely.

	* src/am29xxxxx_aux.c, cdl/flash_am29xxxxx_v2.cdl: add optional
	support for certain Atmel chips which have a peculiar
	implementation of CFI.

2005-08-17  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/flash_am29xxxx_v2.cdl: Expand burst size description
	in line with strata driver's example.
	Provide new
	CYGIMP_DEVS_FLASH_AMD_AM29XXXXX_V2_LEAVE_INTERRUPTS_ENABLED
	and CYGHWR_DEVS_FLASH_AMD_AM29XXXXX_V2_CACHED_ONLY options
	to provide better control of when to enable/disable interrupts
	or caches. Taken from the Strata flash example.
	* include/am29xxxxx_dev.h: Declare cyg_at49xxxx_softlock, _hardlock
	and _unlock variants.
	* src/am29xxxxx.c: Define AT49 locking commands.
	Provide AM29_UNCACHE_ADDRESS in line with the Strata driver,
	to be controlled by the above new CDL options, in place of
	AM29_P2V.
	* src/am29xxxxx_aux.c: Provide AT49 lock status definition.
	Provide AT49 softlock/hardlock/unlock API functions and
	underlying implementation functions.
	Adopt AM29_UNCACHED_ADDRESS rename.
	* doc/am29xxxxx.sgml: Update documentation to cover AT49xxxx
	locking operations and above new CDL options.
	
2005-06-12  Bart Veer  <bartv@ecoscentric.com>

	* src/am29xxxxx_aux.c (cyg_am29xxxxx_program): remove unnecessary
	loops variable
	* cdl/flash_am29xxxxx_v2.cdl: minor reorganization to put the
	important config option first
	* doc/am29xxxxx.sgml: document the important config options

2005-04-12  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/flash_am29xxxxx_v2.cdl: Reduce erase burst loop duration a little
	again, but not as much as before the previous change.

2005-04-06  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/flash_am29xxxxx_v2.cdl: Increase default
	CYGNUM_DEVS_FLASH_AMD_AM29XXXXX_V2_ERASE_BURST_DURATION as it's
	far too small for decent hardware with instruction caches that
	can cache the tight loop checking the flash device. Otherwise
	the flash device keeps spending all its time entering and leaving
	erase suspend mode and not doing real work. Better too high now
	and optimised later by application designers, than sometimes too
	low and often not work.	

2005-02-23  Bart Veer  <bartv@ecoscentric.com>

	* doc/am29xxxxx.sgml: bring up to date.

2005-01-19  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/am29xxxxx_aux.c (am29_hw_erase): Handle interleaved
	(parallel) flash correctly when one device finishes before another.
	(am29_hw_program): Similar.
	(cyg_am29xxxxx_program): Use assert correctly.
	
	* src/am29xxxxx.c (AM29_NEXT_DATUM_32): Use cyg_uint32, not
	cyg_uint16.
	
2004-12-02  Bart Veer  <bartv@ecoscentric.com>

	* src/am29xxxxx.c, include/am29xxxxx_dev.h: <cyg/io/flash_priv.h>
	no longer exists, use <cyg/io/flash_dev.h> instead.

2004-11-29  Bart Veer  <bartv@ecoscentric.com>

	* include/am29xxxxx_dev.h, src/am29xxxxx.c: eliminate
	hwr_map_error() support, no longer needed
	
	* include/am29xxxxx_dev.h, src/am29xxxxx.c, src/am29xxxxx_aux.c:
	The dummy init/query/lock/unlock functions have been moved to the
	generic flash package. That also now exports an anonymizer
	function.

2004-11-25  Bart Veer  <bartv@ecoscentric.com>

	* cdl/flash_am29xxxxx_v2.cdl, src/am29xxxxx.c,
	src/am29xxxxx_aux.c: this driver can manage the flash and
	interrupts itself, without support from the generic flash code.
        Erase suspend/resume have now been implemented, and program
	operations only write a few words at a time between re-enabling
	interrupts.

2004-11-22  Bart Veer  <bartv@ecoscentric.com>

	* include/am29xxxxx_dev.h, src/am29xxxxx.c, src/am29xxxxx_aux.c,
	doc/am29xxxxx.sgml: implement changes to the interface between the
	generic flash code and the device drivers.
	* include/am29xxxxx_dev.h: rename cyg_block_info to
	cyg_flash_block_info

2004-11-21  Bart Veer  <bartv@ecoscentric.com>

	* doc/am29xxxxx.sgml: describe CDL implications for custom locking
	functions and additional devices.
	
	* cdl/flash_am29xxxxx_v2.cdl: CYGHWR_IO_FLASH_DEVICE_V2 is now
	implicit

2004-11-05  Bart Veer  <bartv@ecoscentric.com>

	* New AM29xxxxx flash driver created

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2004, 2005, 2006, 2007, 2008 Free Software Foundation, Inc.
// Copyright (C) 2004, 2005, 2006, 2007, 2008 eCosCentric Limited           
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================