2009-07-03  Nick Garnett  <nickg@ecoscentric.com>

	* src/stm32_flash.c (stm32_flash_init): Add tests for connectivity
	line devices.

2009-04-06  Simon Kallweit  <simon.kallweit@intefo.ch>

	* src/stm32_flash.c:
	stm32_flash_get_block_info() now computes correct block base
	address. HSI is enabled for flash erase/program as stated in the
	manual. Some cleanup.

2008-12-19  Simon Kallweit  <simon.kallweit@intefo.ch>

	* src/stm32_flash.c:
	Hardcoded flash and block sizes as the debug registers are not
	readable by user software.

2008-11-04  Simon Kallweit  <simon.kallweit@intefo.ch>

	* src/stm32_flash.c:
	Fixed detection on early silicon.

2008-10-07  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/flash_stm32.cdl:
	* include/stm32_flash.h:
	* src/stm32_flash.c:
	New package -- support for STM32 on-chip flash.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2008 Free Software Foundation, Inc.                        
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================