2006-11-02  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/spi_eb55.cdl: 
	* include/spi_eb55.h: Tidied up PCSDEC support, not needed any
	more.

2006-10-05  Nick Garnett  <nickg@ecoscentric.com>

	* include/spi_eb55.h: Added additional bus number parameter to
	relevant macros.

2005-08-04  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/spi_eb55.cdl:
	* include/spi_eb55.h:
	* src/spi_eb55.c:
	Initial import into eCosCentric repository.

2004-08-31  Savin Zlobec  <savin@elatec.si> 

	* cdl/spi_eb55.cdl:
	Added a require for 4 to 16 decoder of chip select signals option.
	* src/spi_eb55.c:
	Defined time between two transfers.

2004-08-27  Savin Zlobec  <savin@elatec.si> 

	* cdl/spi_eb55.cdl:
	* include/spi_eb55.h:
	* src/spi_eb55.c:
	Atmel AT91EB55 SPI devices.   	 



//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================