2009-01-31  Bart Veer <bartv@ecoscentric.com>

	* cdl/hal_arm_aim711.cdl: update compiler flags for gcc 4.x

2009-01-24  Bart Veer <bartv@ecoscentric.com>

	* cdl/hal_arm_aim711.cdl: switch from arm-elf-gcc to
	arm-eabi-gcc. Remove -mno-short-load-words.

2008-11-20  Bart Veer  <bartv@ecoscentric.com>

	* misc/redboot_ROMRAM_visionsystems.ecm:
	CYGSEM_HAL_VIRTUAL_VECTOR_CLAIM_CACHE has been expunged from the
	common HAL.

2005-06-11  John Dallaway  <jld@ecoscentric.com>

	* include/pkgconf/mlt_arm_aim711_ram.ldi: Add RELOCS, .got and
	.eh_frame sections to the memory layout.

2004-06-07  Roland Cassebohm <roland.cassebohm@visionsystems.de>

        * src/aim711_misc.c: 
        The I2C transfer routine waits now while the bus is busy
        instead of just return an error.

2004-04-28  Roland Cassebohm <roland.cassebohm@visionsystems.de>

	* include/plf_aux.h:
	* include/plf_io.h:
        Removed plf_aux.h, instead put the prototypes of the functions
        in plf_io.h.

2004-04-28  Roland Cassebohm <roland.cassebohm@visionsystems.de>

        * src/aim711_misc.c: 
	* include/hal_platform_ints.h:
        Removed unused RedBoot startup code.

2004-04-28  Roland Cassebohm <roland.cassebohm@visionsystems.de>

        * cdl/hal_arm_aim711.cdl: 
	* include/hal_platform_ints.h:
        Added cdl option to get delays between POST codes.

2004-04-27  Roland Cassebohm <roland.cassebohm@visionsystems.de>

        * cdl/hal_arm_aim711.cdl: Fixed typos.

2003-10-02  Roland Cassebohm <roland.cassebohm@visionsystems.de>

	* cdl/hal_arm_aim711.cdl:
        Implement CYGINT_HAL_ARM_BIGENDIAN.
        Use "-mno-short-load-words" in compiler flags to avoid unaligned
        access, which would cause exceptions.

	* include/hal_cache.h:
	* include/hal_diag.h: 

	* include/hal_platform_ints.h: Set HAL_PLATFORM_RESET() to
        hal_reset().

	* include/hal_platform_setup.h: Changed for direct initial 
	SDRAM setup. External IO is maped to 0x3fd0000. Changed LED macros
	to use only the first three bits of PIO.

	* include/plf_io.h:

	* include/plf_stub.h: Remove HAL_STUB_PLATFORM_RESET defines,
        because they are not used anymore.

	* include/pkgconf/mlt_arm_aim711_ram.h: Moved FLASH to 0x2000000 
	and changed the size to 0x200000. Changed size of RAM to 0x800000.
        RedBoot is used as main bootloader. To be sure there is enough
        space in future, the RAM version resevers RAM up to 0x30000.
	* include/pkgconf/mlt_arm_aim711_ram.ldi: Same.
	* include/pkgconf/mlt_arm_aim711_rom.h: Same.
	* include/pkgconf/mlt_arm_aim711_rom.ldi: Same.
	* include/pkgconf/mlt_arm_aim711_romram.h: Same.
	* include/pkgconf/mlt_arm_aim711_romram.ldi: Same.

	* misc/redboot_RAM.ecm:
	* misc/redboot_ROM.ecm:
	* misc/redboot_ROMRAM.ecm:

	* src/hal_diag.c: Implement hal_diag_led() for the diagnostic board
        of the AIM.

	* src/aim711_misc.c:
        Implemented reset functionality of the AIM 711 board.

	New package for the ARM Industrial Module AIM 711 cloned from
	SNDS package.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================