2009-02-12  Nick Garnett  <nickg@ecoscentric.com>

	* misc/redboot_RAM.ecm:
	* misc/redboot_ROM.ecm: Add CYGPKG_ERROR to resolve configure-time
	errors.

2009-01-31  Bart Veer <bartv@ecoscentric.com>

	* cdl/hal_arm_at91_eb55.cdl: update compiler flags for gcc 4.x

2009-01-24  Bart Veer <bartv@ecoscentric.com>

	* cdl/hal_arm_at91_eb55.cdl: switch from arm-elf-gcc to
	arm-eabi-gcc. Remove -mno-short-load-words.

2006-10-31  John Dallaway  <jld@ecoscentric.com>

	* cdl/hal_arm_at91_eb55.cdl: Eliminate a stray double-quote
	char.

2006-10-10  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/hal_arm_at91_eb55.cdl: Added implements for serial devices
	available on this board.

2005-02-01  John Dallaway  <jld@ecoscentric.com>

	* misc/redboot_ROM.ecm, misc/redboot_RAM.ecm: Disable
	CYGBLD_BUILD_REDBOOT_WITH_CACHES for RedBoot builds.

2004-11-19  John Dallaway  <jld@ecoscentric.com>

	* cdl/hal_arm_at91_eb55.cdl: Rely on the inference engine to
	adjust CYGBLD_GLOBAL_CFLAGS and CYGBLD_GLOBAL_LDFLAGS in observation
	of CYGHWR_THUMB and CYGBLD_ARM_ENABLE_THUMB_INTERWORK.
	* misc/redboot_ROM.ecm, misc/redboot_RAM.ecm: Enable
	CYGBLD_ARM_ENABLE_THUMB_INTERWORK for RedBoot builds.

2004-09-16  Andrea Michelotti <amichelotti@atmel.com>

	* include/hal_platform_ints.h: When CYGHWR_HAL_ARM_AT91_FIQ is defined 
	  CYGNUM_HAL_ISR_MIN is equal to zero.
	
2004-08-30  Thomas Koeller  <thomas.koeller@baslerweb.com>

	* cdl/hal_arm_at91_eb55.cdl: Reversed change of 2004-02-12.
	The options moved to the variant hal were not truly common
	amoung all platforms.

2004-05-10  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/hal_arm_at91_eb55.cdl: Pass -n to linker to avoid ELF PHDR
	containing a "truncated" program load address.

2004-04-21  Nick Garnett  <nickg@ecoscentric.com>

	* include/hal_platform_setup.h: Fixed thumb assemble problems by
	adding an ldrc (load register with constant) macro that has
	different behaviour depending on __thumb__ setting.

2004-04-08  Andrew Lunn  <andrew.lunn@ascom.ch>

	* misc/redboot_ROMRAM.ecm: Deleted since this is no longer
	supported.

2004-04-08  Alan Bowman <abowman@synaptics-uk.com>

	* include/pkgconf/mlt_arm_at91_eb55_romram.ldi: Alter rom_vectors
	section to match the startup code for ROMRAM applications

2004-03-12  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/pkgconf/mlt_arm_at91_eb55_mec01ram.ldi: Include .eh_frame
	.got, and reloc sections.
	* include/pkgconf/mlt_arm_at91_eb55_ram.ldi: Ditto.
	* include/pkgconf/mlt_arm_at91_eb55_rom.ldi: Ditto.
	* include/pkgconf/mlt_arm_at91_eb55_romram.ldi: Ditto.

2004-03-01  John Dallaway  <jld@ecoscentric.com>

	* misc/redboot_ROMRAM.ecm: Delete to eliminate ROMRAM RedBoot support.

2004-02-18  John Dallaway  <jld@ecoscentric.com>

	* cdl/hal_arm_at91_eb55.cdl: Observe CYGHWR_THUMB and
	CYGBLD_ARM_ENABLE_THUMB_INTERWORK in calculating the default
	values for CYGBLD_GLOBAL_CFLAGS and CYGBLD_GLOBAL_LDFLAGS.

2004-02-12  Jani Monoses <jani@iv.ro>

	* cdl/hal_arm_at91_eb55.cdl: Move configuration options 
	common to all AT91 EB boards up to AT91 variant .cdl.
	
2004-01-23  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/hal_arm_at91_eb55.cdl: Add new option
	CYGHWR_HAL_ARM_AT91_EB55_MEC01_RAM to allow use of MEC01
	extension RAM for linking.
	(CYGHWR_MEMORY_LAYOUT): use mec01 mlt files if above option selected.
	(CYGHWR_MEMORY_LAYOUT_LDI): Ditto.
	(CYGHWR_MEMORY_LAYOUT_H): Ditto.
	(CYGPRI_HAL_ARM_AT91_EB55_MEM_SEGMENTS): New CDL to set RAM segment
	count in redboot package.

	* include/hal_platform_setup.h (_InitMemory): Map MEC01 memory.

	* src/eb55_misc.c (cyg_plf_memory_segment): New function. Called
	by RedBoot to determine RAM segments.

	* include/pkgconf/mlt_arm_at91_eb55_mec01ram.h: New file. Used when
	CYGHWR_HAL_ARM_AT91_EB55_MEC01_RAM enabled.
	* include/pkgconf/mlt_arm_at91_eb55_mec01ram.ldi: Ditto.
	* include/pkgconf/mlt_arm_at91_eb55_ram.h: Define sram and mec01ram
	regions.
	* include/pkgconf/mlt_arm_at91_eb55_rom.h: Ditto.
	* include/pkgconf/mlt_arm_at91_eb55_romram.h: Ditto.
	* include/pkgconf/mlt_arm_at91_eb55_ram.ldi: Define mec01ram region.
	* include/pkgconf/mlt_arm_at91_eb55_rom.ldi: Ditto.
	* include/pkgconf/mlt_arm_at91_eb55_romram.ldi: Ditto.

2003-12-16  Gary Thomas  <gary@mlbassoc.com>

	* misc/redboot_ROMRAM.ecm: 
	CYGNUM_FLASH_WORKSPACE_SIZE is no longer used.

2003-09-30 Jani Monoses <jani@iv.ro> 

	* cdl/hal_arm_at91_eb55.cdl: Interfaces are already implemented by
	AT91 variant .cdl, do not duplicate them here.
	
2003-07-15  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/hal_platform_ints.h (HAL_PLATFORM_RESET): Actually use
	hal_at91_reset_cpu().

2003-05-12  Nick Garnett  <nickg@balti.calivar.com>

	* cdl/hal_arm_at91_eb55.cdl: 
	* include/plf_io.h: 
	* include/hal_platform_setup.h: 
	* include/hal_platform_ints.h: 
	* include/pkgconf/mlt_arm_at91_eb55_ram.ldi: 
	* include/pkgconf/mlt_arm_at91_eb55_ram.h: 
	* include/pkgconf/mlt_arm_at91_eb55_rom.ldi: 
	* include/pkgconf/mlt_arm_at91_eb55_rom.h: 
	* include/pkgconf/mlt_arm_at91_eb55_romram.ldi: 
	* include/pkgconf/mlt_arm_at91_eb55_romram.h: 
	* src/eb55_misc.c: 
	New HAL added to support the Atmel EB55 board. Adapted from the
	EB40 and EB40A HALs by Thomas Koeller and Tim Drury.


//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2003, 2004, 2005 Free Software Foundation, Inc.
// Copyright (C) 2004, 2005 eCosCentric Limited                             
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================