2008-05-06  John Dallaway  <jld@ecoscentric.com>

	* doc/pci.sgml: Refer to the PCI Database.

2004-11-03  David Vrabel  <dvrabel@arcom.com>
	 
	 * src/pci.c (cyg_pci_configure_device): Fix bug which caused
	 memory resources to be not allocated.
	
2004-10-13  David Brennan <eCos@brennanhome.com>

	* src/pci.c: Added include of cyg/infra/diag.h to fix compiler
	warning.

2004-10-12  Mark Salter  <msalter@redhat.com>

	* cdl/io_pci.cdl (CYGPKG_IO_PCI_CONFIGURE_INTLINE): New option.
	* src/pci.c (cyg_pci_translate_interrupt): Don't write INT LINE
	register unless CYGPKG_IO_PCI_CONFIGURE_INTLINE defined.

2004-10-08  John Dallaway  <jld@ecoscentric.com>

	* tests/pci1.c: Add a newline at end of "No PCI devices found"
	diagnostic messages.

2004-09-18  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/pci.c: Add much more debugging, particularly of BARs, controlled
	by new CYGPKG_IO_PCI_DEBUG_BAR define. 
	(cyg_pci_configure_device): Use base_size, not base_address to determine
	if BAR should be skipped. Some devices can have reported valid memory BARs
	with a base address of 0 before sizing.

2004-08-31  Mark Salter  <msalter@redhat.com>

	* src/pci.c (cyg_pci_translate_interrupt): Write vector number into
	INT_LINE register.
	(cyg_pci_get_device_info): Add mechanism for HALs to specify certain
	BARs to be ignored.
	* include/pci_hw.h (CYG_PCI_IGNORE_BAR): New macro.
	* doc/pci.sgml: Add info on HAL_PCI_IGNORE_BAR.

2004-01-14  Nick Garnett  <nickg@calivar.com>

	* src/pci.c (cyg_pci_get_device_info): Added fix for devices that
	only implement the bottom 16 bits of an IO BAR. This is allowed by
	the standard but is very rare and mostly present in older devices
	only. Without this cyg_pci_allocate_io_priv() gets confused.

2004-01-09  David Vrabel  <dvrabel@arcom.com>
        
	* src/pci.c (cyg_pci_find_device): Remove debug message.

2003-11-27  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/pci.c (cyg_pci_find_device): Removed a debug print which should
	not be there and is causing an warning.

2003-11-18  Manu Sharma  <manu.sharma@ascom.com>

        * src/pci.c : Additional changes in cyg_pci_get_device_info, 
        cyg_pci_set_device_info and cyg_pci_configure_device to be able
        to support non-contiguous BARs.

2003-09-29  Nick Garnett  <nickg@balti.calivar.com>

	* src/pci.c (cyg_pci_get_device_info): Removed check for inactive
	BARs since the requirement for the BARs to be contiguous has been
	relaxed in more recent versions of the PCI standard.

2003-08-08  Gary Thomas  <gary@mind.be>

	* include/pci.h: Add CYGARC_PCI_DMA_ADDRESS() macro - used to
	map CPU addresses to ones usable by PCI masters.

2003-02-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/io_pci.cdl: Fix doc link.

2003-02-21  Gary Thomas  <gary@mlbassoc.com>

	* src/pci.c (cyg_pci_get_device_info): While scanning active
	devices, remember the I/O and memory addresses they use.  This
	allows for new devices to be added which will not conflict.

2003-02-20  Gary Thomas  <gary@mlbassoc.com>

	* tests/pcihdr.h: Update to latest published version.

2002-05-14  Jesper Skov  <jskov@redhat.com>

	* tests/pci1.c: Fix warning.

2002-02-13  Hugo Tyson  <hmt@redhat.com>

	* doc/pci.sgml: Tidy up some typos and PROGRAMLISTING width
	issues.

2002-02-11  Mark Salter  <msalter@redhat.com>

	* doc/pci.sgml: Brought docs up to date with current code.

2002-01-31  Mark Salter  <msalter@redhat.com>

	* src/pci.c (cyg_pci_init): Set default memory and io bases here
	as the HAL_PCI_ALLOC_BASE_* macros may not be static values.

2002-01-21  Mark Salter  <msalter@redhat.com>

	* src/pci.c (cyg_pci_get_device_info): Fix setting of upper 32 bits
	for 64-bit BAR.

2001-09-28  Gary Thomas  <gthomas@redhat.com>

	* src/pci.c (cyg_pci_find_next): 
	* include/pci.h: Allow platforms to restrict PCI bus/device ranges.

2001-08-22  Gary Thomas  <gthomas@redhat.com>

	* src/pci.c: 
	printf() is no longer a part of RedBoot.  Thus all programs
	must use diag_printf() and related functions instead.

2001-02-28  Hugo Tyson  <hmt@redhat.com>

	* tests/pci1.c (pci_scan): Added a new function to re-scan the
	device list after configuring to let a human confirm that we truly
	are seeing distinct devices - ie. do they retain their distinct
	resource allocations in the BARs?  This was useful to me in
	investigating a recalcitrant target...

2001-02-02  Jesper Skov  <jskov@redhat.com>

	* tests/pci2.c (pci_test): Removed bogus check for 1MB IO limit.

2001-01-10  Jesper Skov  <jskov@redhat.com>

	* src/pci.c (cyg_pci_get_device_info): Do correct casting of
	header_type. Do not make assumptions about structure layout.

	* tests/pcihdr.h: Updated.

2001-01-02  Hugo Tyson  <hmt@redhat.com>

	* include/pci.h: Define new API to perform more generalized matching
	on device properties.

	* src/pci.c (cyg_pci_find_matching): New API implementation.

2000-12-21  Mark Salter  <msalter@redhat.com>

	* include/pci_hw.h: Add platform hook so certain devices
	can be skipped by generic PCI io code. This is a workaround
	for a hw problem where configuration space cycles on some
	devices cause a bus lockup.
	
	* src/pci.c (cyg_pci_find_next): Use platform hook to ignore
	certain devices during device search.

2000-12-02  Gary Thomas  <gthomas@redhat.com>

	* src/pci.c: 
	* cdl/io_pci.cdl: Add CDL to control debug prints.

2000-11-30  Gary Thomas  <gthomas@redhat.com>

	* src/pci.c (cyg_pci_find_next): Improve debug prints when
	scanning the bus, showing vendor and device code for each slot.

2000-11-19  Gary Thomas  <gthomas@redhat.com>

	* src/pci.c (cyg_pci_find_device): Don't update 'devid' if no
	suitable devices found.  This allows for simpler rescan for
	multiple device types.

2000-11-12  Gary Thomas  <gthomas@redhat.com>

	* src/pci_hw.c: 
	* src/pci.c: Layout changes require <pkgconf/hal.h>

2000-11-06  Jonathan Larmour  <jlarmour@redhat.com>

	* src/pci.c (cyg_pci_find_next): Conditionalize debug printfs

2000-11-04  Mark Salter  <msalter@redhat.com>

	* src/pci.c (cyg_pci_get_device_info): Add bridge support. Handle
	already configured devices.
	(cyg_pci_set_device_info): Add bridge support.
	(cyg_pci_find_next): Support device id with valid bus number
	combined with CYG_PCI_NULL_DEVFN.
	(cyg_pci_configure_device): Return true if device already configured.
	Fixed for devices which use no BARs.
	(cyg_pci_allocate_io_priv): Remove bogus limit check.
	(cyg_pci_configure_bus): New function to recursively configure a
	bus and its subordinate bases.

	* include/pci_cfg.h: Added bridge definitions.
	(CYG_PCI_CFG_BAR_5): Corrected.

	* include/pci.h (CYG_PCI_NULL_DEVFN): Define.
	(cyg_pci_device): Add bridge support. Add num_bars. Add
	declaration for cyg_pci_configure_bus.
	(CYG_PCI_MAX_BUS): Increase to (arbitrary) 8.

2000-03-28  John Dallaway  <jld@cygnus.co.uk>

	* cdl/io_pci.cdl:

	Adjust documentation URLs.

2000-01-31 Simon FitzMaurice  <sdf@cygnus.co.uk>
  * cdl\io_pci.cdl:

  Adjust help URLs in line with new doc layout.
  
2000-01-28 Simon FitzMaurice  <sdf@cygnus.co.uk>
  * cdl\io_pci.cdl:

  Adjust help URLs in line with new doc layout.
  
2000-01-19  Hugo Tyson  <hmt@cygnus.co.uk>

	* cdl/*.cdl: Add descriptions to a number of options &c which were
	lacking same, also tidied up other typos as noticed en passant.

1999-12-21  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* cdl/io_pci.cdl (CYGPKG_IO_PCI): Relevant to more than one platform
	so reparent under IO package
	(CYGPKG_IO_PCI_CFLAGS_REMOVE): Fix display line typo

1999-11-03  John Dallaway  <jld@cygnus.co.uk>

	* cdl/io_pci.cdl: Define build options.

1999-09-24  Jesper Skov  <jskov@cygnus.co.uk>

	* tests/pci2.c (pci_test): Replaced CYG_ASSERT with CYG_TEST_CHECK

1999-09-10  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/io_pci.h: Reparent under CYGPKG_IO - this is used under
	more than one target now and the library itself is generic.

1999-08-25  Jesper Skov  <jskov@cygnus.co.uk>

	* src/pci.c (cyg_pci_init): Made it idempotent.

	* tests/pci1.c:
	* tests/pci2.c:
	* src/pci.c: 
	* include/pci.h: 
	All functions that deal with addresses in PCI space now use PCI
	ADDRESS types.
	
1999-08-24  Jesper Skov  <jskov@cygnus.co.uk>

	* tests/pci1.c: 
	* tests/pci2.c: 
	* include/pci.h: 
	* src/pci.c:
	Handle requests for memory regions in 64bit space.
	
1999-08-24  Jesper Skov  <jskov@cygnus.co.uk>

	* tests/pci1.c: Added more output, resource allocation, debug help
	(enable devices).

	* src/pci.c (cyg_pci_find_next): Handle multi-function devices.

	* include/pci_cfg.h (CYG_PCI_CFG_COMMAND_ACTIVE): Added MASTER.
	Added HEADER_TYPE definitions.

1999-08-23  Nick Garnett  <nickg@cygnus.co.uk>

	* tests/pci1.c: Fixed a couple of bugs in the vendor/device/class
	table search code.

1999-08-23  Jesper Skov  <jskov@cygnus.co.uk>

	* tests/pcihdr.h: [Added]
	* tests/pci1.c: Added Vendor/Device ID description output.

	* include/pci_cfg.h: Added vendor and class IDs.
	Also added Prog/IF IDs.

1999-08-19  Nick Garnett  <nickg@cygnus.co.uk>

	* tests/pci1.c (pci_test): Added printf() of class_rev code to
	output of bus scan.

	* include/pci.h (CYG_PCI_MAX_FN): Increased to 8.

1999-08-19  Jesper Skov  <jskov@cygnus.co.uk>

	* src/pci.c (cyg_pci_allocate_memory, cyg_pci_allocate_io):
	Check that device is inactive. Ensure that 1MB limits (IO/MEM1MB)
	are observed.

	* tests/pci2.c (pci_test): Added tests of io/mem allocators.

1999-08-17  Jesper Skov  <jskov@cygnus.co.uk>

	* tests/pci2.c (pci_test): Added (empty for now)
	* tests/pci1.c: Added API checks.
	* include/pci.h: Fixed typo.

	* include/pci.h (CYG_PCI_NULL_DEVID): Changed initializer.
	* src/pci.c (cyg_pci_find_next): Correct check for initializer.

	* tests/pci1.c: Added.
	Fixed output.

	* include/pci_cfg.h: 
	* include/pci.h: 
	* include/pci_hw.h: 
	* src/pci_hw.c: 
	* src/pci.c: 
	Renamed cyg_pci_config_interrupt to cyg_pci_translate_interrupt.
	Untabified.
	
1999-08-16  John Dallaway  <jld@cygnus.co.uk>

	* cdl/io_pci.cdl:

	Parent PCI library package under package on which it depends.

1999-08-16  John Dallaway  <jld@cygnus.co.uk>

	* include/pkgconf/io_pci.h:

	Parent PCI package under package on which it depends.

1999-08-16  Jesper Skov  <jskov@cygnus.co.uk>

	* include/pci.h: 
	* src/pci.c (cyg_pci_config_interrupt): 
	* include/pci_hw.h:
	* src/pci_hw.c (cyg_pcihw_config_interrupt): 
	Added interrupt configuration functions.
	
1999-08-13  Jesper Skov  <jskov@cygnus.co.uk>

	* include/pci_cfg.h:
	* include/pci.h: 
	* src/pci_hw.c:
	* src/pci.c:
	Extended cyg_pci_device and API.
	Renamed HAL macros.
	Put physical address in base_map.

	(cyg_pci_get_device_info): Fix switch. Clear base_size when device
	enabled.

1999-08-12  Jesper Skov  <jskov@cygnus.co.uk>

	* include/pci_hw.h:
	* include/pci_cfg.h:
	* include/pci.h: 
	* src/pci_hw.c: 
	* src/pci.c:
	Renamed some registers. Fixed some bad arguments. Added forgotten
	externCs.
	cyg_pci_configure_device fleshed out a bit.
	
	* First half-empty files checked in.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2004, 2008 Free Software Foundation, Inc.
// Copyright (C) 2004, 2008 eCosCentric Limited                             
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================