2009-02-04  Bart Veer  <bartv@ecoscentric.com>

	* src/watchdog.cxx: switch to CYG_INIT_DEV_WATCHDOG init priority.

2007-06-21  Bart Veer  <bartv@ecoscentric.com>

	* tests/watchdog_reset.cxx (watchdog_thread): only disable the
	cache if the hardware allows it.

2007-05-31  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/watchdog.cdl: watchdog_reset test is irrelevant if watchdog
	doesn't reset on timeout.

2005-09-26  Bart Veer  <bartv@ecoscentric.com>

	* tests/watchdog_reset.cxx (watchdog_thread): disable interrupts
	around cache manipulation.

2004-06-14  John Dallaway  <jld@ecoscentric.com>

	* cdl/watchdog.cdl: Move the CYGINT_WATCHDOG_IMPLEMENTATIONS
	contraint to the cdl_interface block for correct display under
	the eCos Configuration Tool. Tidy display strings.

2004-05-10  Nick Garnett  <nickg@ecoscentric.com>

	* src/watchdog.cxx: Added prioritization to static watchdog instance.

2003-11-05  Bob Koninckx <bob.koninckx@mech.kuleuven.ac.be>

	* src/watchdog.cxx: 
	* include/watchdog.hxx: 
	* include/watchdog.h: New file - add "C" API for watchdog functions.

2003-04-03  Thomas Koeller  <thomas.koeller@baslerweb.com>

	* cdl/watchdog.cdl: Turned 'wallclock' into 'watchdog' in string.

2003-04-02  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/watchdog.cdl: Watchdog implementation requirement should be
	in package, not interface itself. *Note* must be requires, not
	active_if otherwise turning off the emulated watchdog means you
	can never turn it on again!

2000-05-31  Jesper Skov  <jskov@redhat.com>

	* tests/watchdog.cxx: fix comment.

	* tests/watchdog2.cxx: 
	* cdl/watchdog.cdl: 
	watchdog2 tests timeout is not too fast (safe for both types of
	watchdog semantics).
	
	* tests/watchdog_reset.cxx: 
	* src/emulate.cxx:
	* include/watchdog.hxx:
	Fixed compile errors.

	* cdl/watchdog.cdl: Only build test if the watchdog does not reset
	the board.
	Added build option for interactive reset test.

2000-05-30  Jesper Skov  <jskov@redhat.com>

	* tests/watchdog_reset.cxx: 
	* tests/watchdog.cxx: 
	* src/emulate.cxx: 
	* src/watchdog.cxx: 
	* include/watchdog.hxx: 
	* cdl/watchdog.cdl: 
	Moved to io/watchdog.

2000-01-31 Simon FitzMaurice  <sdf@cygnus.co.uk>
  * cdl/watchdog.cdl:

  Adjust help URLs in line with new doc layout.

2000-01-28 Simon FitzMaurice  <sdf@cygnus.co.uk>
  * cdl/watchdog.cdl:

  Adjust help URLs in line with new doc layout.

2000-01-19  Hugo Tyson  <hmt@cygnus.co.uk>

	* cdl/*.cdl: Add descriptions to a number of options &c which were
	lacking same, also tidied up other typos as noticed en passant.

1999-11-03  John Dallaway  <jld@cygnus.co.uk>

	* cdl/watchdog.cdl: Define build options.

1999-09-09  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* include/pkgconf/watchdog.h: Rename CYGPKG_HAL_MN10300_SIM to
	CYGPKG_HAL_MN10300_AM31_SIM

1999-09-07  Jesper Skov  <jskov@cygnus.co.uk>

	* include/pkgconf/watchdog.h:
	* src/aeb1.cxx: [added]
	* src/PKGconf.mak:
	* tests/PKGconf.mak:
	Added watchdog driver for AEB-1 board.

1999-09-07  Jesper Skov  <jskov@cygnus.co.uk>
        PRs 20427, 20428, 20432
	* tests/PKGconf.mak (TESTS): Clear on targets that reset the
	board.

1999-09-01  Jesper Skov  <jskov@cygnus.co.uk>
	* cdl/watchdog.cdl: 
	* include/pkgconf/watchdog.h: 
	* src/PKGconf.mak: 
	* src/sh.cxx: 
	Added watchdog driver for SH.

1999-08-27  Jesper Skov  <jskov@cygnus.co.uk>
	* include/pkgconf/watchdog.h: 
	* src/PKGconf.mak: 
	* src/ebsa285.cxx: 
	Added watchdog device for 21285.

	* tests/watchdog_reset.cxx: 
	* tests/PKGconf.mak (TESTS):
	Added test for watchdog devices that reset the board.

1999-08-24  Nick Garnett  <nickg@cygnus.co.uk>

	* src/mn10300.cxx: Turn watchdog off in Cyg_Watchdog::trigger() to
	prevent it repeating.

1999-08-18  Nick Garnett  <nickg@cygnus.co.uk>

	* include/pkgconf/watchdog.h: Made test for use of a non-emulated
	watchdog more generic for MN10300 targets.

	* src/emulate.cxx: 
	* include/watchdog.hxx (class Cyg_Watchdog):
	Added get_resolution() to return maximum time, in nanoseconds,
	between calls to reset().

	* tests/watchdog.cxx: 
	Modified to use the value returned from get_resolution() to
	control the timing of reset() calls.
	
	* src/mn10300.cxx: 
	Added support for AM33 variant. Since the AM33 can only provide a
	maximum watchdog cycle time of 621ms, this has motiviated the
	addition of the get_resolution() call described above.

1999-07-14  Jesper Skov  <jskov@cygnus.co.uk>

	* src/mn10300.cxx: 
	* src/emulate.cxx: 
	Include pkgconf/kernel.h.

1999-04-21  Gary Thomas  <gthomas@cygnus.co.uk>

	* tests/watchdog.cxx: The 'keep alive' message was interfering
	with the watchdog measurement.  Some rearrangement fixes this.

1999-04-20  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/watchdog.cxx: 
	Restrict number of loops, and number of seconds per loop when we
	detect we are in a simulator. Do this instead of changing the
	value of one_sec in the simulator, since this invalidates the test
	somewhat.
	Output occasional messages to reassure the user that the test is
	still running.
	Fix for PR 19865

1999-04-14  Jesper Skov  <jskov@cygnus.co.uk>

	* tests/watchdog.cxx (cyg_start): Added workaround for PR 17974.

1999-04-12  John Dallaway  <jld@cygnus.co.uk>

	* include/pkgconf/watchdog.h: Add cdl_package doc attribute.

1999-04-08  Gary Thomas  <gthomas@cygnus.co.uk>

	* tests/watchdog.cxx: PR 19773 - Loop over first test for better 
	coverage. Print some additional messages, especially if failure 
	detected.  Reset watchdog after installing handler.
	(watchdog_thread): Capture fail time before printing message.

1999-04-07  Jesper Skov  <jskov@cygnus.co.uk>
        PR 19667
	* tests/watchdog.cxx (cyg_start): 
	Changed to use the new Cyg_Thread constructor.

1999-03-22  Hugo Tyson  <hmt@cygnus.co.uk>

	* tests/watchdog.cxx: 
	Use CYGNUM_HAL_STACK_SIZE_TYPICAL for the stack size instead of
	CYGNUM_HAL_MINIMUM_STACK_SIZE.

1999-03-12  Hugo Tyson  <hmt@cygnus.co.uk>

	* tests/watchdog.cxx: 
	Deal with CYGNUM_HAL_MINIMUM_STACK_SIZE requirement.

1999-03-04  Gary Thomas  <gthomas@cygnus.co.uk>

	* include/pkgconf/watchdog.h: Make package stand-alone (no "DEVICES")

1999-02-20  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/mn10300.cxx: 
	Change CYG_VECTOR_WATCHDOG to CYGNUM_HAL_INTERRUPT_WATCHDOG in line
	with HAL changes.
	General QA improvements

1999-02-03  Jesper Skov  <jskov@cygnus.co.uk>
        PR 19034
	* tests/watchdog.cxx: Reduced run-time on SIM.

1998-12-17  Jesper Skov  <jskov@cygnus.co.uk>

	* tests/watchdog.cxx: Do NOP test if kernel RTC disabled.

1998-10-23  Jesper Skov  <jskov@cygnus.co.uk>

	* tests/watchdog.cxx (cyg_start): Reduce test time on TX39 SIM.

	* include/pkgconf/watchdog.h: Use emulatation code for MN10300
	SIM.

Tue Oct 20 15:52:46 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* src/mn10300.cxx: 
	Include <pkgconf/watchdog.h> so that we get CYGIMP_WATCHDOG_EMULATE
	defined appropriately

	* src/PKGconf.mak:
	Remove unnecessary override of PKGCONF_CXXFLAGS

1998-09-26  Bart Veer  <bartv@cygnus.co.uk>

	* include/pkgconf/watchdog.h:
	PR17501: When using the emulation there is a requirement on the
	kernel clock. This has been added to the configuration data. The
	mn10300 hardware implementation does not have this requirement,
	but there is no easy way to express this at present.

1998-09-12  Bart Veer  <bartv@cygnus.co.uk>

	* include/pkgconf/watchdog.h:
	Added missing descriptions (PR 17184)

1998-09-02  Bart Veer  <bartv@cygnus.co.uk>

	* include/pkgconf/watchdog.h:
	Added minimal configuration data.

1998-09-01  Nick Garnett  <nickg@cygnus.co.uk>

	* src/mn10300.cxx:
	Added include for <cyg/kernel/sched.inl>, for scheduler lock and
	unlock functions.

	* src/PKGconf.mak:
	Added mn10300.cxx to COMPILE for mn10300.

	* include/pkgconf/watchdog.h:
	Default to using real hardware on MN10300.

Fri Aug 28 09:42:26 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/watchdog.cxx:
	Rename int main(argc, argv) to void cyg_start( void ) under the
        new entry point system. Therefore also remove return code.

Tue Aug 18 16:51:24 1998  Jonathan Larmour  <jlarmour@cygnus.co.uk>

	* tests/watchdog.cxx: 
	Move inclusion of thread.inl to before sched.hxx to prevent inline
	warnings

1998-08-14  Nick Garnett  <nickg@cygnus.co.uk>

	* src/emulate.cxx:
	Added include for cyg/kernel/sched.inl.

1998-07-31  Nick Garnett  <nickg@cygnus.co.uk>

	* src/PKGconf.mak:
	Added mn10300.cxx to COMPILE list.

	* src/mn10300.cxx:
	Completed implementation using MN10300 watchdog timer.

	* include/watchdog.hxx:
	Renamed 'register' functions to 'install'. Added install() and
	uninstall() to Cyg_Watchdog_Action class.

	* include/pkgconf/watchdog.h:
	Added this file to contain watchdog config options.

1998-07-29  Nick Garnett  <nickg@cygnus.co.uk>

	* include/watchdog.hxx, src/emulate.cxx: 
	Created initial versions of watchdog device.

// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2009 Free Software Foundation, Inc.
// Copyright (C) 2004, 2005, 2007 eCosCentric Limited                                   
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####