2009-01-26  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/ctype.c: Allow to run if CYGPKG_LIBC_STARTUP isn't there.
	* tests/i18nmb.c: Ditto.
	* tests/setlocale.c: Ditto.

2008-12-18  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/locale.cxx: Tidy change of 2007-07-02 and add more const
	string warning cleanups.

2007-09-17  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/i18n.cdl: locale.cxx needs libc string functions.

2007-07-02  Gary Thomas  <gary@mlbassoc.com>

	* src/locale.cxx: Add (char *) casts to make GCC/4.2.x happy.

2006-09-25  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/i18n.cdl (YGSEM_LIBC_I18N_PER_THREAD_MB): Implement
	CYGINT_KERNEL_THREADS_DATA_EXTRA as we need per-thread data slots.

2006-08-28  Sergei Gavrikov  <w3sg@SoftHome.net>

	* src/wcstombs.cxx (wcstombs): unused variable removed.

2006-08-11  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/wcstombs.cxx (wcstombs): Previous change should have
	disregarded 'n'. Now fixed. Thanks to Klaas Gadeyne.

2006-08-10  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/wcstombs.cxx (wcstombs): Follow Single Unix Spec
	and if string is NULL, return chars that would have been
	returned.

2005-07-30  Andrew Lunn  <andrew.lunn@ascom.ch>

	* tests/i18nmb.c (main): Really silence the warnings.

2004-02-17  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/i18n.cdl: Add newlib style ctype implementation.
	CYGSEM_LIBC_I18N_PER_THREAD_MB can be inactive when no kernel.
	* include/newlibctype.h: New file.
	* src/newlibctype.cxx: New file.
	* src/ctype.cxx: Don't define functions if newlib style ctype
	chosen instead.

	* src/wctomb.cxx (wctomb): Use correct thread data type.
	* src/mbtowc.cxx (mbtowc): Ditto.
	* src/mblen.cxx (mblen): Ditto.

2003-02-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/i18n.cdl: Fix doc link.

2001-06-28  Jesper Skov  <jskov@redhat.com>

	* tests/i18nmb.c: fix warning.

2001-06-08  Jonathan Larmour  <jlarmour@redhat.com>

	* src/mbtowc_jp.cxx (__mbtowc_jp): Fix nasty bug for mblen(NULL, x);

	Some other cleanups across the board to the below changes before
	checking in.

2001-06-08  Jeff Johnston  <jjohnstn@redhat.com>

	* cdl/i18n.cdl: Added implements CYGINT_ISO_STDLIB_MULTIBYTE. 
	(CYGPKG_LIBC_I18N_LOCALES): New component
	encompassing supported locales.
	(CYGFUN_LIBC_I18N_LOCALE_C_JIS): New configuration
	item to support the new "C-JIS" C/Japanese locale.  Option defines
	CYGINT_LIBC_I18N_MB_REQUIRED.
	(CYGFUN_LIBC_I18N_LOCALE_C_SJIS): Similar except it is "C-SJIS" locale.
	(CYGFUN_LIBC_I18N_LOCALE_C_EUCJP): Ditto except it is "C-EUCJP" locale.
	(CYGSEM_LIBC_I18N_PER_THREAD_MB): New option that determines
	if multibyte functions will keep state data per thread or not.
	(CYGNUM_LIBC_I18N_MAX_LOCALE_NAME_SIZE): Changed legal_values and
	default_value to be dependent on whether the Japanese locales
	were supported or not.
	(CYGPKG_LIBC_I18N_TESTS): Add multibyte test.
	* src/locale.cxx: Moved Cyg_libc_locale_t to internal.h.
	Changed current ctype locale to be externally accessible variable.
	Added MB_CUR_MAX value into locale as well as pointers to mbtowc
	and wctomb functions.
	[CYGINT_LIBC_I18N_MB_REQUIRED]: Added __mb_cur_max external variable.
	(all_locales)[CYGFUN_LIBC_I18N_LOCALE_C_JIS]: New "C-JIS" locale 
	added to list.
	(all_locales)[CYGFUN_LIBC_I18N_LOCALE_C_SJIS]: New "C-SJIS"
	locale.
	(all_locales)[CYGFUN_LIBC_I18N_LOCALE_C_EUCJP]: New "C-EUCJP"
	locale.
	(setlocale)[CYGINT_LIBC_I18N_MB_REQUIRED]: Added setting of __mb_cur_max
	when locale changes ctype category.
	(__get_current_locale_mbtowc_fn): New function.
	* src/mblen.cxx: New file.
	* src/mbtowc.cxx: Ditto.
	* src/mbstowcs.cxx: Ditto.
	* src/wctomb.cxx: Ditto.
	* src/wcstombs.cxx: Ditto.
	* src/mbtowc_jp.cxx: Ditto.
	* src/mbtowc_c.cxx: Ditto.
	* src/internal.h: New internal header file.
	* tests/i18nmb.c: New test case for multibyte functionality.

2000-05-02  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* New package
	Separated original libc out into separate packages on functional
	boundaries.
	Header files are now managed by isoinfra package
	Plenty of cleanups done, but no major functionality changes

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2006, 2007 Free Software Foundation, Inc.
// Copyright (C) 2006, 2007 eCosCentric Limited                             
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================