2009-01-28  Bart Veer  <bartv@ecoscentric.com>

	* tests/getenv.c: N/A in configurations which do not provide
	environ.

2009-01-26  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/abs.c: Allow to run if CYGPKG_LIBC_STARTUP isn't there.
	* tests/atoi.c: Ditto.
	* tests/atol.c: Ditto.
	* tests/bsearch.c: Ditto.
	* tests/div.c: Ditto.
	* tests/getenv.c: Ditto.
	* tests/labs.c: Ditto.
	* tests/ldiv.c: Ditto.
	* tests/qsort.c: Ditto.
	* tests/rand1.c: Ditto.
	* tests/rand2.c: Ditto.
	* tests/rand3.c: Ditto.
	* tests/rand4.c: Ditto.
	* tests/srand.c: Ditto.
	* tests/strtol.c: Ditto.
	* tests/strtoul.c: Ditto.

2008-12-23  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/strtoull.cxx, src/strtoll.cxx, src/strtoul.cxx, src/strtoul.cxx:
	lisp'ify to avoid compiler warnings.

2007-01-12  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/getenv.cxx: Declare environ if CYGPKG_LIBC_STARTUP isn't there
	to do it.

2006-09-25  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/stdlib.cdl (CYGSEM_LIBC_PER_THREAD_RAND): 
	Implement CYGINT_KERNEL_THREADS_DATA_EXTRA as we need per-thread data
	slot.

2005-12-27  Sergei Organov  <osv@javad.com>

	* src/strtod.cxx (Ise): 'd' and 'D' aren't allowed in floating
	formats.

2005-04-11  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/strtod.cxx: No need to explicitly check CYGFUN_LIBC_strtod.

2005-03-28  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/stdlib.cdl: Only build strtod.cxx and strtof.cxx when needed.

2005-02-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/strtof.inl (strtof): Correct implementation to allow for
	strtod returning something that fits in a double but not a float,
	in which case we return an appropriate error.
	* cdl/stdlib.cdl (CYGFUN_LIBC_strtod): Needs errno and errno codes.

2005-02-07  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/strtof.inl: New file. Implements strtof().
	* include/strtox.h: New file. Defines isoinfra prototypes for
	string to float conversion functions, overriding default isoinfra ones.
	* src/strtof.cxx: New file. Provides outline strtof().

	* cdl/stdlib.cdl: Build strtof.cxx. Define override header for
	CYGBLD_ISO_STDLIB_STRCONV_FLOAT_HEADER for isoinfra.
	
2004-08-18  Fredrik Hederstierna  <fredrik@wespot.com>
2004-08-18  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/strtoll.cxx, src/strtoull.cxx: New files. Support for long long
	string conversion.
	* cdl/stdlib.cdl (CYGFUN_LIBC_STDLIB_CONV_LONGLONG): New option
	to build above new files configurably.
	* include/atox.inl: Prototype new functions from above. Add atoll()
	inline.

2004-04-22  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/strtod.cxx (strtod): Fail conversion if no exponent supplied
	despite e/E being present, e.g. "1E".
	Handle overflow of significand correctly.
	Handle border cases near the limits of DBL_MAX/DBL_MIN better.

2004-02-17  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/rand.cxx (srand): Use correct thread data type.
	(rand): Ditto.

2003-02-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/stdlib.cdl: Fix doc link.

2001-06-28  Jesper Skov  <jskov@redhat.com>

	* tests/atoi.c (main): Fix warning.

2001-06-18  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/stdlib.cdl: requires string functions, so say so.

2001-02-14  Jonathan Larmour  <jlarmour@redhat.com>

	* src/rand.cxx: Fix typo

2000-08-03  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* src/getenv.cxx: Revert nickg's change of 2000-06-07. environ is
	meant to be determined by the startup environment (normally in
	CYGPKG_LIBC_STARTUP), not getenv.

2000-07-27  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* cdl/stdlib.cdl: Require CYGINT_ISO_CTYPE because we need the iswhite()
	etc. funs

2000-07-04  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* cdl/stdlib.cdl: Remove all parts of malloc implementation and
	move to new separate package CYGPKG_MEMALLOC

	* src/malloc.cxx, tests/malloc1.c, tests/malloc2.c, tests/malloc3.c,
	tests/realloc.c: remove - moved to CYGPKG_MEMALLOC

2000-06-07  Nick Garnett  <nickg@cygnus.co.uk>

	* tests/realloc.c: Include correct pkgconf file.

	* src/getenv.cxx: Removed externC from definition of environ, so
	that is actually gets defined.

2000-05-02  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* New package
	Separated original libc out into separate packages on functional
	boundaries.
	Header files are now managed by isoinfra package
	Plenty of cleanups done, but no major functionality changes

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2004, 2005, 2006, 2007 Free Software Foundation, Inc.
// Copyright (C) 2004, 2005, 2006
2007 eCosCentric Limited                  
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================