2009-03-09  John Dallaway  <john@dallaway.org.uk>

	* cdl/ftpclient.cdl: Reference test executable filenames for
	compatibility with the eCos Configuration Tool.

2006-09-11  Daniel Nri  <daniel.neri@sigicom.se>

	* src/ftpclient.c (send_cmd): Use correct variable in error check.

2005-07-30  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/ftpclient.c (connect_to_server): Use socklen_t to avoid
	compiler warning.

2005-07-13  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/ftpclient1.c (ftp_test): Do delete first to avoid disrupting
	ret code containing number of file bytes.

	* src/ftpclient.c (command): May as well show full command.
	(login): fix spelling.

2005-07-08  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/ftpclient1.c (ftp_test): Try and delete /incoming/passwd
	at the start just in case. Too many old tarballs in the test farm
	are still leaving it behind.

2005-05-26  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/ftpclient.c (ftp_delete): Add support for FTP deletion.
	(opendatasock): Fix potential buf with namespace masking of socket
	's' by a string.
	* include/ftpclient.h: Declare ftp_delete. Make file C++ safe.
	* tests/ftpclient1.c: Tidy output substantially. Fix ftp_put
	success return code test. Delete /incoming/passwd when done.
	Add CYG_TEST_FINISH at end.

2004-10-04  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/ftpclient.c (opendatasock): Don't clobber the socket
	variable with a temporary variable of local scope.

2004-05-24  Gary Thomas  <gary@mlbassoc.com>

	* src/ftpclient.c: 
	* include/ftpclient.h:
	* cdl/ftpclient.cdl: Add new functions 'ftp_get_var()' and 'ftp_put_var()'
	which allow for streams of data instead of fixed buffers.

2003-07-02  Daniel Néri  <daniel.neri@sigicom.se>

	* src/ftpclient.c (send_cmd): Fix typo in error message.
	(opendatasock): Use snprintf instead of sprintf.

2003-04-28  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/ftpclient.c (connect_to_server): Added support for
	IPv6. This meant changing from using the PORT command to using
	EPRT, when setting up the data connection. EPRT is protocol 
	independant. 
	* tests/ftpclient1.c (ftp_test): Added tests which use IPv6
	addresses. Fixed a few minor bugs with format strings.
	* doc/ftpclient.sgml: Mention we support IPv6 and DNS.
	
2003-02-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/ftpclient.cdl: Add doc link.

2002-08-06  Andrew Lunn <andrew.lunn@ascom.ch>

	* src/ftpclient.c: Send "quit" not "quit " to keep some servers
	  happy.  Also deal with multi line replies correctly.
	
2002-02-22  Hugo Tyson  <hmt@redhat.com>

	* doc/ftpclient.sgml: New file.  Document it.

2001-12-04  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/ftpclient.c: Allow it to compile!

2001-11-04  Andrew Lunn  <andrew.lunn@ascom.ch>
	
	* First version. Implements an FTP client which can get and put 
	  files on a server. 
 	
//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2005, 2007 eCosCentric Limited                             
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2003, 2009 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================