2009-03-09  John Dallaway  <john@dallaway.org.uk>

	* cdl/sntp.cdl: Reference test executable filenames for	compatibility
	with the eCos Configuration Tool.

2007-05-31  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/sntp1.c (net_test): ntp servers usually broadcast
	every 64 seconds in fact, so set default multicast wait
	time to 70.

2007-05-24  Nick Garnett  <nickg@ecoscentric.com>

	* doc/sntp.sgml: Update description to reflect changes in
	relationship between POSIX CLOCK_REALTIME and the wallclock.

2006-11-08 Andre Mas <andrejohn.mas@gmail.com>

        * src/sntp.c: Removed optional KeyIdentifer and MessageDigest
        fields, which weren't being used, and caused certain servers
        not to respond when these fields were included with null values.

2005-10-06  Jonathan Larmour  <jifl@eCosCentric.com>

	* doc/sntp.sgml: Epoch is 1970 not 1900.

2005-08-11  Nick Garnett  <nickg@ecoscentric.com>

	* tests/sntp1.c: Adjusted to work correctly with a system clock
	rate other than 100Hz.

2005-07-30  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/sntp.c: Compiler warning fixes.

2004-02-26 Yuxin Jiang <yjiang@matrics.com>

	* src/sntp.c: When a new server is added to the list of unicast
	servers don't wait 30 minutes before querying it for the first
	time.

2003-10-15  Dan Jakubiec  <djakubiec@yahoo.com>
            Andrew Lunn   <andrew.lunn@ascom.ch>

	* src/sntp.c: Added DHCP support for SNTP unicast mode.
	* src/sntp.cdl: Added DHCP support for SNTP unicast mode.
	* src/sntp.h: Removed UDP port constant.
	* src/sntp1.c: Added test code for SNTP unicast mode.
	* src/sntp.sgml: Added documentation for SNTP unicast mode.

2003-09-29  Dan Jakubiec  <firstname.lastname@systech.com>

	* src/sntp.c: Added support for SNTP unicast mode.
	* src/sntp.h: Added support for SNTP unicast mode.
	* src/sntp.cdl: Added support for SNTP unicast mode.

2003-05-19  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/sntp.c: Added support for IPv6 multicast NTP packets.

2003-04-09  Michael Checky  <Michael_Checky@Thermoking.com>

	* src/sntp.c: In function sntp_fn() changed 'version' to
	'new_srv.version' in the CYG_TRACE1() call.

2003-02-25  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/sntp.h: Include <cyg/infra/cyg_type.h> for __externC.

2003-02-25  Gary Thomas  <gary@mlbassoc.com>

	* tests/sntp1.c (net_test): Strip the trailing "\n" making it more
	  readable.
	
2003-02-25  Andrew Lunn  <andrew.lunn@ascom.ch>

	* doc/sntp.sgml: Added license banner and added missing </para>
	* include/sntp.h (cyg_sntp_start): C++ safe
	* cdl/sntp.cdl: Stricture requirements and same description as in
  	  ecos.db.  Only build the test if CYGPKH_NET_BUILD_HW_TESTS
	* tests/sntp1.c (net_test): Check we have the required
	  packages. Require the time to be within 90 days of the build
	  date of the test
		
	
2003-02-16  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/sntp.c: First import of SNTP client code.
	* include/sntp.c: Ditto
	* test/sntp1.c: Ditto
	* cdl/sntp.cdl: Ditto
	* doc/sntp.sgml: Ditto

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2004, 2005, 2007 eCosCentric Limited                       
// Copyright (C) 2003, 2009 Free Software Foundation, Inc.                        
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================