2005-02-15  Jonathan Larmour  <jifl@eCosCentric.com>

	* current.ect: Provide inferred default for
	CYGBLD_ISO_STDLIB_STRCONV_FLOAT_HEADER.

2004-04-15  Jonathan Larmour  <jifl@eCosCentric.com>

	* current.ect: Provide default for CYGBLD_ISO_STDIO_FILEOPS_HEADER
	and CYGBLD_ISO_STDIO_FILEPOS_HEADER.

2003-02-25  Andrew Lunn       <andrew.lunn@ascom.ch>
	
	* Added the Simple Network Time Protocol (SNTP) Client

2003-02-14  Jonathan Larmour  <jifl@eCosCentric.com>

	* Move files from templates/net/ to templates/old_net/

	* current.ect: Update inferred values.

2001-11-27  Jonathan Larmour  <jlarmour@redhat.com>

	 current.ect: Provide default for CYGBLD_ISO_STRING_BSD_FUNCS_HEADER

2001-09-27  Jonathan Larmour  <jlarmour@redhat.com>

	* current.ect: Don't include uitron. Not appropriate for base net
	template.

2001-09-26  Jesper Skov  <jskov@redhat.com>

	* current.ect: DNS header moved.

2001-09-24  Jesper Skov  <jskov@redhat.com>

	* current.ect: Added DNS package.

2001-08-21  Jonathan Larmour  <jlarmour@redhat.com>

	* current.ect: Pre-infer CYGBLD_ISO_PMUTEXTYPES_HEADER.

2000-11-03  Jonathan Larmour  <jlarmour@redhat.com>

	* current.ect: Update inferred values for current CDL

2000-08-03  Gary Thomas  <gthomas@redhat.com>

	* current.ect: Ethernet drivers have moved.

2000-07-04  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* current.ect: Add memalloc package

2000-06-07  Nick Garnett  <nickg@cygnus.co.uk>

	* current.ect: Modified to work with ISOINFRA package, divided
	LIBC and fileio package.

2000-05-31  Jesper Skov  <jskov@redhat.com>

	* current.ect: renamed watchdog package.

2000-04-07  Hugo Tyson  <hmt@cygnus.co.uk>

	* ecos.db: Re-organize device packages.  This is a massive change
	involving deleting all the sources for serial and ethernet drivers
	from where they used to live in
	    packages/io/serial/current/src/ARCH/PLATFORM.[ch]
	    packages/net/drivers/eth/PLATFORM/current/src/...
	and reinstating them in
	    packages/devs/serial/ARCH/PLATFORM/current/src/...
	    packages/devs/eth/ARCH/PLATFORM/current/src/...

	All these new packages are properly defined in ecos.db, and are
	all of type "hardware" so that a "target" can grab them.
	
	This directory layout is descriptive of the devices we have right
	now, arch and platform are separate levels just to make it easier
	to navigate in the filesystem and similar to the HAL structure in
	the filesystem.

	It is *not* prescriptive of future work; for example, the mythical
	common highly-portable 16550 serial driver which works on many
	targets would be called "devs/serial/s16550/current", or a serial
	device for a particular board (cogent springs to mind) that can
	work with different CPUs fitted is "devs/serial/cogent/current".

	Changelogs have been preserved and replicated over all the new
	packages, so that no history is lost.

	The contents of individual source files are unchanged; they build
	in just the same emvironment except for a very few cases where the
	config file name changed in this movement.

	Targets in ecos.db have been redefined to bring in all relevant
	hardware packages including net and serial drivers (but the newly
	included packages are only active if their desired parent is
	available.)
	
	The names of CDL options (and their #defines of course) stay the
	same for the serial drivers, for backward compatibility.

	* templates/*/current.ect: these have had CYGPKG_IO_SERIAL added
	rather than it being in (almost) all target definitions.
	
2000-04-05  Jesper Skov  <jskov@redhat.com>

	* current.ect: Wallclock moved.

2000-02-08  Gary Thomas  <gthomas@cygnus.co.uk>

	* templates/net: New template with optional network package.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================