2009-09-10  Bart Veer  <bartv@ecoscentric.com>

	* common/eCosStd.h: cope with some mingw tchar.h omissions.

2009-04-16  Bart Veer  <bartv@ecoscentric.com>

	* common/eCosThreadUtils.cpp (CeCosThreadUtils): distinguish
	between VC++ and mingw builds

2006-03-29  John Dallaway  <jld@ecoscentric.com>

	* common/eCosSocket.h: Specify CeCosSerial as a friend class to
	enable compilation with GCC 4.x. [ Bugzilla 1000207 ]

2004-12-14  John Dallaway  <jld@ecoscentric.com>

	* common/Subprocess.cpp: Define _GNU_SOURCE to ensure that stdlib.h
	provides Unix98 PTY declarations on Red Hat Linux 7.3.

2004-12-03  John Dallaway  <jld@ecoscentric.com>

	* common/Subprocess.cpp (CSubprocess::CreateProcess): Try the Unix98
	PTY scheme in addition to the BSD scheme. Recent Linux kernels may
	be built without legacy PTY support.

2003-04-30  John Dallaway  <jld@ecoscentric.com>

	* common/eCosStd.h: Update version string to "2.net".
	  Use WSAEWOULDBLOCK under Cygwin.

2003-02-12  Bart Veer  <bartv@ecoscentric.com>

	* common/configure, common/Makefile.in:
	Regenerate after acinclude.m4 update

2003-01-25  John Dallaway  <jld@ecoscentric.com>

	* common/Collections.cpp: #include <winsock2.h> early for Cygwin
	builds to eliminate fd_set compiler warning

	* common/eCosSocket.cpp: Add newline at end of file to eliminate
	compiler warning


2003-01-20  John Dallaway  <jld@ecoscentric.com>

	* common/eCosThreadUtils.cpp:
	Use "try" rather than "__try" for Cygwin builds.

	* common/eCosStd.h:
	#include winsock2.h and process.h for Cygwin builds.

	* common/Properties.cpp:
	Use MIN macro rather than min() for portability.

2002-08-03  Bart Veer  <bartv@ecoscentric.com>

	* common/Makefile.am, common/configure.in, common/acinclude.m4:
	Rework host-side autoconf support

2000-09-15  Jesper Skov  <jskov@redhat.com>

	* common/Makefile.in: Regenerated.
	* common/configure: Ditto.

	* common/eCosSocket.h: Made SSReadResult enum public.

	* common/Makefile.am: Added autoconf/make support.
	* common/Makefile.in: Ditto.
	* common/configure: Ditto.
	* common/configure.in: Ditto.
	* common/acinclude.m4: Ditto.
	* common/aclocal.m4: Ditto.

	* common/wcharunix.h (_tperror): Make putenv convert String to
	char*.

2000-08-01  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* common/eCosSerial.h: 
	* common/eCosSerial.cpp:
	Add support for setting RTSCTS, DSRDTR and XONXOFF flow control
	for both win32 and unix

2000-04-14 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\Subprocess.cpp
    common\Subprocess.h

  Always attempt to kill a process explicitly (don't let Cygwin processes linger)

2000-04-13 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosSerial.cpp
    common\eCosSocket.cpp
    common\eCosTrace.cpp

  Tidy up timestamp output.
    
2000-04-11 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\Collections.cpp
    common\Collections.h
    common\Properties.cpp
    common\Properties.h
    common\eCosStd.h
    common\eCosThreadUtils.cpp
    common\eCosThreadUtils.h
    common\eCosTrace.cpp
    common\eCosTrace.h
    common\wcharunix.h
    win32\CTUtils.cpp

  General tidy-up.  

2000-03-13 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\Collections.cpp
    common\Properties.cpp
    common\eCosStd.cpp
    common\eCosStd.h
    common\eCosThreadUtils.cpp
    common\eCosThreadUtils.h
    common\eCosTrace.cpp

	Mark UNIX sections of code as such.
	Correct bug in GetBuffer() - always allow enough space for allocation of *old* string.

2000-03-10 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosStd.cpp
    common\eCosStd.h
    common\eCosThreadUtils.cpp

	Move CeCosTrace class to its own file

  * win32\IntegerEdit.cpp

  Eliminate compilation warning
    
	*	win32\SubProcess.cpp

	Start on UNIX implementation

2000-03-08 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosThreadUtils.cpp

  Correct compilation problem on UNIX.
	
2000-03-08 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosThreadUtils.cpp
    common\eCosThreadUtils.h

  Add name argument to RunThread calls for debugging.

2000-03-08 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosStd.cpp
    common\eCosStd.h
    common\eCosThreadUtils.cpp
    common\eCosThreadUtils.h

	Avoid potential race condition in RunThread.

2000-03-07 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\Collections.cpp
    common\Collections.h
    common\Properties.cpp
    common\eCosStd.cpp
    common\eCosStd.h
    common\eCosThreadUtils.cpp
    win32\SubProcess.cpp
    win32\SubProcess.h

	Use std::vector directly instead of StringArray, PtrArray
	Introduce common command-line processing to CeCosTestUtils
	Tidy output and trace functions and move to CeCosTrace
	CSubprocess Run functions now return thread id and pass instead of this pointer to message callbacks.

2000-03-03 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\Collections.cpp
    common\Collections.h
    common\Properties.cpp
    common\Properties.h
  
  Thread-related eCosTest code extracted to new class CeCosThreadUtils  

2000-03-02 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\Properties.cpp
    common\Properties.h
    win32\SubProcess.cpp
    win32\SubProcess.h

  Migrate more classes to Utils from eCosTest.
  Use common CSubprocess class implementation.

2000-02-29 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\Properties.h : CeCosTestUtils::String->String

  * win32\CSHDialog.cpp
    win32\CSHPropertyPage.cpp
    win32\CSHPropertySheet.cpp : guard against unexpected rclick position

  * win32\FileName.cpp : eliminate compilation warnings

2000-02-25 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\Properties.cpp
    common\Properties.h

 Allow prefix to be supplied to support serialization chaining.

2000-02-22 Simon FitzMaurice <sdf@redhat.co.uk>
  * win32\IntegerEdit.cpp
    win32\IntegerEdit.h

  Keep spin control sized according to parent.

2000-02-21 Simon FitzMaurice <sdf@redhat.co.uk>
  * win32/MultiLineEditDialog.cpp

  Add WS_TABSTOP to controls.

2000-02-21 Simon FitzMaurice <sdf@redhat.co.uk>
  * win32/IntegerEdit.cpp

  Do not allow thousands in spin ctrl.

2000-02-18 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\Properties.h

  CreateKey should be Win32-only

2000-02-16 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\Properties.cpp
    common\Properties.h

  Add support for defining platforms.

2000-02-15 Simon FitzMaurice <sdf@redhat.co.uk>
  * win32\CSHPropertyPage.cpp
    win32\CSHPropertySheet.cpp

  Prevent recursion via OnWndMsg

  * win32\FileName.cpp
    win32\FileName.h

  Add bFailIfAlreadyExists parameter to CreateDirectory()