2009-09-10  Bart Veer  <bartv@ecoscentric.com>

	* common/eCosTest.cpp (CygPath): cope with mingw/msys paths.

2009-02-09  John Dallaway  <john@dallaway.org.uk>

	* common/eCosTest.cpp (CygPath): Accommodate UNC file paths.

	* common/eCosTest.cpp (GetSizes): Accommodate an empty command prefix
	string.

2007-10-25  Gary Thomas  <gary@mlbassoc.com>

	* common/eCosTest.h: Remove class qualifier - no longer legal
	in GCC-4.x

2006-09-06  John Dallaway  <jld@ecoscentric.com>

	* common/eCosTestUtils.cpp, common/eCosTestUtils.h,
	  common/eCosTest.h: Further tweaks to function prototypes for
	recent GCC.

2006-07-10  John Dallaway  <jld@ecoscentric.com>

	* common/eCosTestUtils.cpp, common/eCosTestUtils.h: Tweak function
	prototypes for GCC 3.4.4.

2003-04-11  John Dallaway  <jld@ecoscentric.com>

	* common/eCosTestPlatform.cpp (CeCosTestPlatform::Load): Return
	true since it's not a problem if there are no platforms defined.

	* unix/Makefile: Allow ser_filter to build under Cygwin.

2003-02-21  John Dallaway  <jld@ecoscentric.com>

	* common/eCosTestPlatform.cpp (CeCosTestPlatform::Load): Allow an
	extra character for string termination when retrieving registry
	key names.

2003-02-13  John Dallaway  <jld@ecoscentric.com>

	* common/eCosTestPlatform.cpp:
	Look for all persistent application settings under
        "HKEY_CURRENT_USER\Software\eCos Configuration Tool\"
	for consistency.

2003-02-05  John Dallaway  <jld@ecoscentric.com>

	* common/eCosTest.cpp (CygPath): Get the cygdrive prefix from
	the registry.

2003-01-20  John Dallaway  <jld@ecoscentric.com>

	* common/eCosTestPlatform.cpp (CProperties::CreateKey):
	"sizeof TCHAR" -> "sizeof (TCHAR)" for GNU headers.

2001-02-20  Jonathan Larmour  <jlarmour@redhat.com>

	* common/eCosTestClient.cpp (LocateExecutables): Add /sbin and
	/usr/sbin to path before trying to run fuser.

2000-09-28  Jesper Skov  <jskov@redhat.com>

	* common/eCosTestSerialFilter.cpp (CMD_TestBinary): Reset counter
	for each test so the failure data is the same from two different
	runs of the test.

2000-09-15  Jesper Skov  <jskov@redhat.com>

	* common/ser_filter.cpp (main): Don't require ResourceServer.

	* common/Makefile.am: Added ser_filter handling.
	* common/Makefile.in: Ditto.
	* common/configure: Ditto.
	* common/configure.in: Ditto.
	* common/eCosTest.cpp: Fix typo.

2000-08-16  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* common/ser_filter.cpp (main): Clean up warning

2000-08-08  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* common/eCosTestSerialFilter.h: Update flow_cfg_t values for correct
	target settings

2000-08-01  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* common/eCosTestSerialFilter.cpp (PrintHex): Print out more printable
	chars
	(SetConfig): Support flow control
	(ParseConfig): Support target setting of flow control
	(CMD_TestBinary): Don't output XON/XOFF. Output 255 chars not 256
	to make buffer problems more obvious.

	* common/eCosTestDownloadFilter.h: Allow SET_VALUE to set optional args
	* common/eCosTestSerialFilter.h: Allow SET_VALUE to set optional args
	Also add flow_cfg_t type and flags member in ser_cfg_t for flow control

2000-07-24  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* common/eCosTestSerialFilter.cpp (FilterFunctionProper): 
	Store output for tracing up so it is output a packet at a time.
	As well as clarifying the output, it is required when sending to
	GDB to prevent the trace 'O' packets in the middle of target packets.
	(CMD_TestBinary): Delay to allow target to read in checksum. This
	prevents overruns before finishing reading the checksum masking
	the real cause of the problem.
	(CeCosTestSerialFilter): Initialise stored trace buffer members

	* common/eCosTestSerialFilter.h: Add trace buffer members for above
	to CeCosTestSerialFilter

2000-06-19  John Dallaway  <jld@redhat.com>

	* unix/Makefile:

	Link with -lposix4 under Solaris for sched_yield().

2000-06-16  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* common/eCosTestDownloadFilter.cpp: Remove RCS id tags
	* common/eCosTestMonitorFilter.cpp: Ditto
	* common/eCosTestSerialFilter.cpp: Ditto

2000-06-15  John Dallaway  <jld@redhat.com>

	* common/eCosTest.cpp:

	Modify CeCosTest construvtor to use GetEnvironmentVariable()
	rather than _tgetenv() under Win32. For some unknown reason,
	_tgetenv() is not returning the correct version of PATH.

	* common/eCosTestPlatform.cpp:

	Modify SaveToRegistry() to save all test platform attributes.

2000-05-03  Bart Veer  <bartv@redhat.com>

	* common/permtest.cxx (find_ptest):
	Do a little bit of searching for the permutation file.
	Catch errors and give a diagnostic, rather than aborting because
	of an uncaught C++ exception.

2000-04-14 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp : do not carry forward values for skipped fields in reset strings
  * common\eCosTest.cpp : Avoid overflow in socket timeouts
    
2000-04-13  Jesper Skov  <jskov@redhat.com>

	* unix/Makefile: add randfile

2000-04-13  Jesper Skov  <jskov@redhat.com>

	* common/eCosTestDownloadFilter.cpp: Cast Write arguments to void*.

2000-04-13 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp
    common\eCosTest.cpp
    common\eCosTestClient.cpp

  Ensure socket timeout matches on_off/off_on delay for reset
  Correct parsing of eCosTestClient delay args.
  Use remote resource to determine baud rate for default download timeout.

2000-04-13 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp
    common\eCosTest.cpp
    common\eCosTest.h
    common\eCosTestClient.cpp
    common\eCosTestServer.cpp
    common\eCosTestUtils.cpp
    common\rgdb.cpp
    common\summlog.cpp
    common\x10reset.cpp
    win32\eCosTest.dsp

  Tidy up reset output.
  Police use of -f and -r switches more accurately.
  Set default timeout in all cases.

2000-04-11 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp
    common\ResetAttributes.h
    common\ResourceServer.cpp
    common\TestResource.cpp
    common\TestResource.h
    common\X10.h
    common\X10d.cpp
    common\eCosTest.cpp
    common\eCosTest.h
    common\eCosTestClient.cpp
    common\eCosTestDownloadFilter.cpp
    common\eCosTestDownloadFilter.h
    common\eCosTestMonitorFilter.cpp
    common\eCosTestMonitorFilter.h
    common\eCosTestSerialFilter.cpp
    common\eCosTestSerialFilter.h
    common\eCosTestServer.cpp
    common\eCosTestUtils.cpp
    common\eCosTestUtils.h
    common\resetall.cpp
    common\rgdb.cpp
    common\ser_filter.cpp
    common\stat.cpp
    common\summlog.cpp
    common\x10reset.cpp
    unix\Makefile
    win32\eCosTest.dsp
    win32\Amplicon\AmpliconD.cpp

  General tidy-up.

2000-04-10  Bart Veer  <bartv@redhat.com>

	* common/permtest.cxx (main):
	Add diagnostics callbacks to database initialization.

2000-03-20  John Dallaway  <jld@cygnus.co.uk>

	* win32/eCosTest.dsp:

	Add common/eCosTestMonitorFilter.h and
	common/eCosTestMonitorFilter.cpp to the project.

2000-03-16  Jesper Skov  <jskov@redhat.com>

	* common/eCosTestMonitorFilter.h:
	* common/eCosTestMonitorFilter.cpp:
	* common/ser_filter.cpp:
	* unix/Makefile (common_sources): 
	Added monitor filter and new -m option to ser_filter. This allows
	simple monitoring of the traffic between host and target.

2000-03-15  John Dallaway  <jld@cygnus.co.uk>

	* common/eCosTest.cpp:

	Modify RunGdb() to sleep 500ms if there is no message.

2000-03-13 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResourceServer.cpp
    common\TestResource.cpp
    common\eCosTest.cpp
    common\eCosTestClient.cpp
    common\eCosTestSerial.cpp
    common\eCosTestSerial.h
    common\eCosTestSocket.cpp
    common\eCosTestSocket.h
    common\eCosTestUtils.cpp
    common\randfile.cpp
    common\rgdb.cpp
    common\ser_filter.cpp

	Mark UNIX sections of code as such.
	Correct behavior of eCosTestClient when give directory as argument.
	A couple of allocations -> stack for simplicity.

2000-03-10 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp
    common\ResourceServer.cpp
    common\X10.cpp
    common\TestResource.cpp
    common\TestResource.h
    common\X10d.cpp
    common\eCosTest.cpp
    common\eCosTest.h
    common\eCosTestDownloadFilter.cpp
    common\eCosTestSerial.cpp
    common\eCosTestServer.cpp
    common\eCosTestSocket.cpp
    common\rgdb.cpp
    common\ser_filter.cpp
    common\x10reset.cpp
    unix\Makefile
    win32\eCosTest.dsp
    win32\Amplicon\AmpliconD.cpp
		
	Move CeCosTrace class to its own file
	Increase Time type to 64 bits to avoid signedness problems
  Remove priority latch functionality

  * common\eCosTestUtils.cpp
    common\eCosTestUtils.h

  Make CommandLine() UNICODE-compliant


  * common\summlog.cpp

	Remove hack designed to cater for incorrectly terminated output lines

  * win32\SingleCPU.cpp

	Provide ability to run on named processor

  * common\eCosTestClient.cpp

	Improve recognition of non-executable files on UNIX

2000-03-09 Simon FitzMaurice <sdf@redhat.co.uk>
  * win32\SingleCPU.cpp

  Avoid a performance problem with bash which, when left to its own devices, is slow on multi-processor machines.

2000-03-09  John Dallaway  <jld@cygnus.co.uk>

	* common/eCosTest.cpp,
	  common/eCosTest.h:

	Use 'REMOTE_SIM' as the platform type identifier for
	remote simulators.

2000-03-09  Bart Veer  <bartv@redhat.com>

	* common/permtest.cxx (main):
	Add an explicit call to resolve_all_conflicts(), although I am not
	yet sure under what circumstances this would be necessary.

2000-03-08 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosTestClient.cpp

  Correct logic error - - allow multiple threads only when non-local

2000-03-08  Bart Veer  <bartv@redhat.com>

	* common/configure.in (cyg_ac_infra_libdir):
	Fix typo detected by Solaris build


2000-03-08 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\summlog.cpp

  Eliminate compiler warnings on UNIX.

2000-03-08 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosTestClient.cpp

	Prevent locally running clients loading from resource server.

2000-03-08 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosTest.cpp
    common\summlog.cpp

  Ensure that gdb output is terminated by a newline and that summlog initializes target list correctly.

2000-03-08 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp
    common\X10d.cpp
    common\eCosTest.cpp
    common\eCosTestClient.cpp
    win32\Amplicon\AmpliconD.cpp

  Add name argument to RunThread calls for debugging.
	Do not allow wait for SuckTheadfunc in reset to time out - thread already has a timeout

  * win32\eCosTest.dsw : 	Adapt to new location of cdl.dsp
  * common\summlog.cpp : ensure eCosTest::Init() and Term() are called


2000-03-08 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp
    common\ResourceServer.cpp
    common\X10d.cpp
    common\eCosTest.cpp
    common\eCosTest.h
    common\eCosTestClient.cpp
    common\eCosTestServer.cpp
    common\eCosTestUtils.cpp
    common\eCosTestUtils.h
    common\resetall.cpp
    common\rgdb.cpp
    common\ser_filter.cpp
    common\stat.cpp
    common\summlog.cpp
    common\x10reset.cpp
    win32\Amplicon\AmpliconD.cpp

	Eliminate GarbageCollector class in favor of CeCosTest::Init() and CeCosTest::Term()
	Fix UNICODE problems in eCosTestUtils

2000-03-08  Bart Veer  <bartv@redhat.com>

	* common/permtest.cxx (process_startup):
	Look for CYGHWR_HAL_STARTUP as well as CYG_HAL_STARTUP

2000-03-08  John Dallaway  <jld@cygnus.co.uk>

	* win32/eCosTest.dsw:

	Use relocated cdl project file.

2000-03-07  Bart Veer  <bartv@redhat.com>

	* common/permtest.cxx (process_startup):
	If a target does not have a CYG_HAL_STARTUP option, ignore any
	attempts to set the startup.

2000-03-07 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp
    common\ResetAttributes.h
    common\ResourceServer.cpp
    common\TestResource.cpp
    common\TestResource.h
    common\X10.cpp
    common\X10d.cpp
    common\eCosTest.cpp
    common\eCosTest.h
    common\eCosTestClient.cpp
    common\eCosTestDownloadFilter.cpp
    common\eCosTestDownloadFilter.h
    common\eCosTestSerial.cpp
    common\eCosTestSerial.h
    common\eCosTestSerialFilter.cpp
    common\eCosTestSerialFilter.h
    common\eCosTestServer.cpp
    common\eCosTestSocket.cpp
    common\eCosTestSocket.h
    common\eCosTestUtils.cpp
    common\eCosTestUtils.h
    common\resetall.cpp
    common\rgdb.cpp
    common\ser_filter.cpp
    common\stat.cpp
    common\summlog.cpp
    common\x10reset.cpp
    win32\eCosTest.dsw
    win32\Amplicon\AmpliconD.cpp

	Use std::vector directly instead of StringArray, PtrArray
	Introduce common command-line processing to CeCosTestUtils
	Tidy output and trace functions and move to CeCosTrace

2000-03-03 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\TestResource.h
    common\eCosTest.cpp
    common\eCosTest.h

  Adjust for UNIX compiler requirements.

2000-03-03 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp
    common\TestResource.cpp
    common\X10d.cpp
    common\eCosTest.cpp
    common\eCosTest.h
    common\eCosTestClient.cpp
    common\eCosTestUtils.cpp
    common\eCosTestUtils.h
    unix\Makefile
    win32\eCosTest.dsp
    win32\Amplicon\AmpliconD.cpp

  Thread-related code extracted to new class CeCosThreadUtils

2000-03-03 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\TestResource.cpp
    common\TestResource.h
    common\eCosTest.cpp

  Eliminate memory leaks.
  Allow resources to be properly reused for benefit of Resource Tool.

2000-03-02 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp
    common\ResetAttributes.h
    common\ResourceServer.cpp
    common\TestResource.cpp
    common\TestResource.h
    common\X10.cpp
    common\X10d.cpp
    common\eCosTest.cpp
    common\eCosTest.h
    common\eCosTestClient.cpp
    common\eCosTestDownloadFilter.cpp
    common\eCosTestDownloadFilter.h
    common\eCosTestSerial.cpp
    common\eCosTestSerial.h
    common\eCosTestSerialFilter.cpp
    common\eCosTestSerialFilter.h
    common\eCosTestServer.cpp
    common\eCosTestSocket.cpp
    common\eCosTestSocket.h
    common\eCosTestUtils.cpp
    common\eCosTestUtils.h
    common\resetall.cpp
    common\rgdb.cpp
    common\ser_filter.cpp
    common\stat.cpp
    common\stdafx.cpp
    common\stop.cpp
    common\summlog.cpp
    common\x10reset.cpp
    unix\Makefile
    win32\eCosTest.dsp
    win32\Amplicon\AmpliconD.cpp

  Introduce flexible reset scheme.
  Migrate more classes to Utils from eCosTest.
  Introduce collections.h for String, StringArray etc...
  Use common CSubprocess class implementation.

2000-02-29 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp : Ensure it compiles on unix

2000-02-29 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp : correct typo
  * win32\eCosTest.dsw : add testtool
        
2000-02-29 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp
    common\ResetAttributes.h
    common\ResourceServer.cpp
    common\TestResource.cpp
    common\TestResource.h
    common\X10d.cpp
    common\eCosTest.cpp
    common\eCosTest.h
    common\eCosTestClient.cpp
    common\eCosTestSerial.cpp
    common\eCosTestSerial.h
    common\eCosTestSerialFilter.cpp
    common\eCosTestServer.cpp
    common\eCosTestSocket.cpp
    common\eCosTestSocket.h
    common\eCosTestStd.h
    common\eCosTestUtils.cpp
    common\eCosTestUtils.h
    common\resetall.cpp
    common\rgdb.cpp
    common\stat.cpp
    common\summlog.cpp
    common\wcharunix.h
    common\x10reset.cpp
    win32\subprocess.cpp
    win32\subprocess.h
    win32\Amplicon\AmpliconD.cpp

  Change to flexible reset scheme.
  CeCosTestUtils::String -> String, CeCosTestUtils::StringArray -> StringArray

2000-02-25 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp
    common\ResetAttributes.h
    common\ResourceServer.cpp
    common\TestResource.cpp
    common\x10reset.cpp

  Use ResetAttributes properties to serialize TestResource.

2000-02-25 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp
    common\ResetAttributes.h
    common\TestResource.cpp
    common\X10.cpp
    common\X10d.cpp
    common\eCosTestClient.cpp
    common\eCosTestServer.cpp
    common\x10reset.cpp
    win32\Amplicon\AmpliconD.cpp

  Reset control string verification fully server-side

2000-02-25 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResetAttributes.cpp
    common\ResetAttributes.h
    common\TestResource.cpp
    common\X10.cpp
    common\X10.h
    common\X10d.cpp
    common\eCosTest.cpp
    common\eCosTestClient.cpp
    common\eCosTestServer.cpp
    common\x10reset.cpp
    win32\Amplicon\AmpliconD.cpp
  
  Normalize control code usage to 0-15, 0-15

2000-02-25 Simon FitzMaurice <sdf@redhat.co.uk>
  * unix/Makefile : update for ResetAttributes

2000-02-25 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\TestResource.cpp
    common\TestResource.h
    common\X10.cpp
    common\X10.h
    common\X10d.cpp
    common\eCosTest.cpp
    common\eCosTestClient.cpp
    common\eCosTestServer.cpp
    common\resetall.cpp
    common\x10reset.cpp
    win32\X10d.dsp
    win32\eCosTest.dsp
    win32\Amplicon\AmpliconD.cpp

  Generalize "X10 reset" to "reset" - introduce ResetAttributes class to hold the details.

2000-02-24 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\TestResource.cpp
    common\TestResource.h
    common\X10.h
    common\X10d.cpp
    common\x10reset.cpp
    win32\eCosTest.dsw

  Add Amplicon to "all" project.
  Fail on reset if comms/tcp port cannot be opened.
  Add -t (timeout on read) param to x10reset

2000-02-24 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\TestResource.cpp
    win32\eCosTest.dsw
    win32\Amplicon\AmpliconD.cpp
    win32\Amplicon\AmpliconD.dsp
    win32\Amplicon\Dio_tc.h
    win32\Amplicon\Dio_tc.lib

  Implement Amplicon reset daemon in C++.

2000-02-23 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\TestResource.cpp
    common\X10d.cpp
    common\eCosTest.cpp
    common\eCosTest.h
    common\eCosTestClient.cpp
    common\eCosTestStd.h
    common\eCosTestUtils.cpp
    common\summlog.cpp
    common\wcharunix.h

  strnccmp -> _tcsicmp

2000-02-23 Simon FitzMaurice <sdf@redhat.co.uk>
  * win32\eCosTest.dsw

  Add "All" utility project.

2000-02-23 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosTest.cpp
    common\eCosTest.h

  Allow HwTypes to be expressed as strings.
    
2000-02-23 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\TestResource.cpp
    common\X10.cpp
    common\X10d.cpp
    common\x10reset.cpp

  Change X10 daemon protocol to allow long delays

2000-02-22 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\TestResource.cpp
    common\eCosTest.cpp
    common\eCosTestClient.cpp
    
  Adjust for Solaris.
  Increase total reset timeout.

2000-02-21 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\TestResource.cpp
    common\TestResource.h
    common\X10.h
    common\eCosTest.cpp
    common\eCosTest.h

  Add "Originator", "Reason", "BoardId", "Email" and "Date" to known resource attributes.
  Add reset timeout attribute.
    
2000-02-18 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosTest.cpp
    common\eCosTest.h

  Changes to support non-gdb execution.

2000-02-17 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosTest.cpp

  Remove incorrect #include

2000-02-16 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\TestResource.cpp
    common\eCosTest.cpp
    common\eCosTest.h

  Add support for defining platforms.

2000-02-14 Simon FitzMaurice <sdf@redhat.co.uk>

  * common\permtest.cxx

  Update copyright headers in files with non-standard extensions :-)

2000-02-14 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResourceServer.cpp
    common\TestResource.cpp
    common\TestResource.h
    common\X10.cpp
    common\X10.h
    common\X10d.cpp
    common\eCosTest.cpp
    common\eCosTest.h
    common\eCosTestClient.cpp
    common\eCosTestDownloadFilter.cpp
    common\eCosTestDownloadFilter.h
    common\eCosTestSerial.cpp
    common\eCosTestSerial.h
    common\eCosTestSerialFilter.cpp
    common\eCosTestSerialFilter.h
    common\eCosTestServer.cpp
    common\eCosTestSocket.cpp
    common\eCosTestSocket.h
    common\eCosTestStd.h
    common\eCosTestUtils.cpp
    common\eCosTestUtils.h
    common\randfile.cpp
    common\resetall.cpp
    common\rgdb.cpp
    common\ser_filter.cpp
    common\stat.cpp
    common\stdafx.cpp
    common\stop.cpp
    common\summlog.cpp
    common\wcharunix.h
    common\x10reset.cpp
    win32\subprocess.cpp
    win32\subprocess.h

  Update copyright headers

2000-02-07 Simon FitzMaurice <sdf@redhat.co.uk>
  * win32\subprocess.cpp

  Fix fix to handle leak.


2000-02-07 Simon FitzMaurice <sdf@redhat.co.uk>
  * win32\eCosTest.dsw

  Add "All" target

  * win32\subprocess.cpp

  Fix handle leak

2000-02-04 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosTestDownloadFilter.cpp
    common\eCosTestSerialFilter.cpp
    common\eCosTestUtils.cpp

  Correct for abnormal behaviour of vsnprintf under NT.

  * win32\permtest.dsp

  Use cdl from v:\ide 

2000-02-01 Simon FitzMaurice <sdf@redhat.co.uk>
  * ecostest\common\TestResource.cpp
    ecostest\common\eCosTest.cpp
    ecostest\common\eCosTest.h
    ecostest\common\eCosTestClient.cpp
    ecostest\common\eCosTestDownloadFilter.cpp
    ecostest\common\eCosTestSerialFilter.cpp
    ecostest\common\eCosTestSocket.cpp
    ecostest\common\eCosTestStd.h
    ecostest\common\eCosTestUtils.cpp
    ecostest\common\eCosTestUtils.h
    ecostest\common\rgdb.cpp
    ecostest\common\summlog.cpp
    ecostest\win32\summlog.dsp

  min->MIN for compilation on UNIX
  CeCosTest::ExecutionParameters gains type as 1st argument
  Performance improvements to summlog

2000-02-01 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResourceServer.cpp 
    common\TestResource.h 
    common\X10.cpp 
    common\X10.h 
    common\X10d.cpp 
    common\eCosTestDownloadFilter.h 
    common\eCosTestSerial.cpp 
    common\eCosTestSerial.h 
    common\eCosTestSerialFilter.h 
    common\eCosTestServer.cpp 
    common\eCosTestSocket.h 
    common\randfile.cpp 
    common\resetall.cpp 
    common\ser_filter.cpp 
    common\stat.cpp 
    common\stdafx.cpp 
    common\stop.cpp 
    common\wcharunix.h 
    common\x10reset.cpp 
    win32\subprocess.cpp 

  Normalize copyright headers.

2000-01-31  Bart Veer  <bartv@redhat.com>

	* common\permtest.cxx (tcl_pkgconf_command):
	Use the default template rather than the all template when
	uItron is disabled. Downgrade an error to a warning to cope
	with the watchdog device not being in the default template.
	
2000-01-28 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosTest.cpp

  Check cancelled status in gdb driving loop.

2000-01-27 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\summlog.cpp

  Ensure pass and inapplic separated in totals for the architectures by perm tables.

2000-01-21 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\resourceserver.cpp

  Efficiency improvements (single send on query)

2000-01-20 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\summlog.cpp

  Separate Pass and NA.
  Fix problem w\ successful results not being counted.

2000-01-19 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosTest.cpp
    common\eCosTestUtils.cpp
    common\eCosTestUtils.h
    common\summlog.cpp

  Attempt to reduce memory usage of summlog.
  Found possible problem - different specs of vsnsprintf on UNIX vs NT.

2000-01-14 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\ResourceServer.cpp
    common\eCosTest.cpp
    common\eCosTestSocket.cpp

  Cygnus -> Red Hat (not copyrights)

  * common\summlog.cpp

  Attempt to fix memory behaviour on UNIX.

2000-01-14 Simon FitzMaurice <sdf@redhat.co.uk>
  * summlog.cpp

  Correct too-late release of string buffer.

2000-01-13 Simon FitzMaurice <sdf@redhat.co.uk>
  * eCosTest.cpp

  Correct overload problem w\ Run

1999-12-23  John Dallaway  <jld@redhat.co.uk>

	* unix\Makefile:

	Use g++ for compilation rather than egcs.

1999-12-23  John Dallaway  <jld@redhat.co.uk>

	* common\eCosTestUtils.h:

	Use '#pragma warning' with Microsoft compiler only.

1999-12-22 Simon FitzMaurice <sdf@redhat.co.uk>
  * unix\makefile

  Add stl library to link  

1999-12-22 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosTestUtils.h
    common\eCosTest.cpp

  Make it compile on UNIX

1999-12-21 Simon FitzMaurice <sdf@redhat.co.uk>
  * win32\eCosTest.dsw

  Remove TestTool (as an MFC project using properties it cannot link against the non-MFC eCosTest library)

  * common\ResourceServer.cpp

  Do not read the files if unchanged since last time

  * common\summlog.cpp

  Remove remote PR lookup functionality

1999-12-17  John Dallaway  <jld@redhat.co.uk>

	* win32\permtest.dsp:

	Generate RTTI when building permtest.

1999-12-17  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* common\permtest.cxx (tcl_value_command): Ensure BoolData options
	are enabled if they are given a value

1999-12-15  John Dallaway  <jld@redhat.co.uk>

	* win32\permtest.dsp:

	New VC++ project.

	* win32\eCosTest.dsw:

	Add the new permtest project to the eCosTest
	workspace.

1999-12-14  John Dallaway  <jld@redhat.co.uk>

	* common\permtest.cxx:

	Further changes to accommodate the recent libCDL
	API changes.

	* common\permtest.cxx:

	Accommodate the recent libCDL API changes.

1999-12-08 Simon FitzMaurice <sdf@redhat.co.uk>
  * common\eCosTest.cpp
    common\eCosTest.h
    common\eCosTestUtils.cpp
    common\eCosTestUtils.h

    Tighter policing of GetBuffer().
    Fix vFormat (needed terminating \0)

1999-12-07 Simon FitzMaurice <sdf@redhat.co.uk>

  * common\TestResource.cpp
    common\TestResource.h
    common\eCosTest.cpp
    common\eCosTest.h
    common\eCosTestClient.cpp
    common\eCosTestSerialFilter.cpp
    common\eCosTestServer.cpp
    common\eCosTestSocket.cpp
    common\eCosTestSocket.h
    common\eCosTestUtils.cpp
    common\eCosTestUtils.h
    common\rgdb.cpp
    common\wcharunix.h
    common\x10reset.cpp
    win32\eCosTest.dsp

  Base string class on STL.
  Use subprocess class (like than in CT)

1999-11-23  John Dallaway  <jld@redhat.co.uk>

	* unix\Makefile:

	Add explicit pattern matching rule for compiling .cpp files.

1999-11-11  Bart Veer  <bartv@redhat.co.uk>

	* common\permtest.cxx:
	Be more tolerant in the data that is accepted, to allow for
	incompatibilities between the old and new worlds.

1999-11-09  Bart Veer  <bartv@redhat.co.uk>

	* common\permtest.cxx
	Replacement for permtest.tcl

	* common\acinclude.m4
	* common\configure.in
	* common\Makefile.am
	* common\configure
	* common\Makefile.in
	* common\aclocal.m4
	Build support for permtest.tcl replacement

1999-10-20  John Dallaway  <jld@redhat.co.uk>

	* win32\eCosTest.dsp, win32\eCosTest.mak,
	  win32\ResourceServer.dsp, win32\ResourceServer.mak:

	Fix intermediate and output directories for the release build.

1999-10-19  Jesper Skov  <jskov@redhat.co.uk>

	* common\X10d.cpp: Allow using '0' as a NOP serial device for the
	reset controller.

	* common\eCosTest.cpp: Send 'quit' to GDB after 'bt'.

1999-10-18  Jesper Skov  <jskov@redhat.co.uk>

	* unix\Makefile [deleted]:
	* unix\Makefile [added]:
	Better makefile.

1999-10-14  Jesper Skov  <jskov@redhat.co.uk>

	* common\ser_filter.cpp: Enabled DL filter as default.

	* common\eCosTestDownloadFilter.h: 
	* common\eCosTestDownloadFilter.cpp:
	* common\eCosTest.cpp (ConnectSocketToSerialThreadFunc): 
	Allow two connections during a session if the first one is a file
	download.
	
	* common\eCosTestServer.cpp: Added missing arg.

1999-10-13  Jesper Skov  <jskov@redhat.co.uk>

	* common\eCosTestDownloadFilter.h: 
	* common\eCosTestDownloadFilter.cpp:
	Use Buffer instead of array for in-buffer. Made its size an
	argument of the info packet.
	Added status to protocol (OK\DL failure\transfer failure)
	
1999-10-11  Jesper Skov  <jskov@redhat.co.uk>

	* common\eCosTest.cpp (ConnectSocketToSerialThreadFunc): Enabled
	download filter.

	* common\eCosTestDownloadFilter.cpp: Fixed a few compiler warnings.

1999-10-08  Jesper Skov  <jskov@redhat.co.uk>

	* unix\makefile: Fixed.

	* common\eCosTest.cpp:
	* common\eCosTest.h:
	* common\eCosTestSocket.cpp:
	* common\eCosTestSocket.h:
	* common\ser_filter.cpp:
	Changed ConectSocketToSerial to take parameter for both serial and
	socket filters.

	* common\eCosDownloadFilter.cpp: [added]
	* common\eCosDownloadFilter.h: [added]
	* common\ser_filter.cpp:
	Added download filter.

1999-10-07  John Dallaway  <jld@redhat.co.uk>

	* common\eCosTest.cpp,
	  common\eCosTest.h:

	New GetGreatestSubkey() function returns the name of
	the subkey of the specified key with the greatest value.

	Modify InitTargetInfoReg() to look in the HKEY_LOCAL_MACHINE
	hierarchy rather than the HKEY_CURRENT_USER hierarchy.

	Modify InitTargetInfo() to construct the platforms registry
	key using GetGreatestSubkey().