Quilt 0.4-Alpha
---------------
Ant Integration works a lot better now.

ClassLoader's actually do their job.  It should
make it work under a much larger set of programs.


Quilt 0.2-Alpha
---------------

Introduced junit.quilt.cover.ball94.B94Registry.
It should run faster than the State Machine durring
execution, but it is slow when generating the report.

The Ant task is looking up.  It should be working
soon, if not now.  I really need to come up with a
way of testing it.

I am using Jakarta Maven (http://jakarta.apache.org/turbine/maven/)
as my build system now.  As such, get the "mquilt" package from
CVS, and get Maven if you would like to build Quilt.


Quilt 0.1.01-Alpha
------------------

Fixed problem with Loop instrumentation.


Quilt 0.1-Alpha
---------------

First public build of Quilt.

Some problems are known, but it
passes all of its Unit Tests.
Enjoy, more releases are around
the corner.