Uses of Class
junit.quilt.cover.generic.ControlFlowGraph

Packages that use ControlFlowGraph
junit.quilt.cover.ball94   
junit.quilt.cover.generic   
junit.quilt.cover.none   
junit.quilt.cover.state   
 

Uses of ControlFlowGraph in junit.quilt.cover.ball94
 

Methods in junit.quilt.cover.ball94 with parameters of type ControlFlowGraph
 void B94ClassLoader.instrumentMethod(InstContext context, ControlFlowGraph graph)
           
 

Uses of ControlFlowGraph in junit.quilt.cover.generic
 

Methods in junit.quilt.cover.generic with parameters of type ControlFlowGraph
abstract  void MethInstClassLoader.instrumentMethod(InstContext context, ControlFlowGraph graph)
          instrumentMethod Override this abstract method to instrument a method.
 void MethInstClassLoader.instrumentEdge(InstContext context, ControlFlowGraph graph, FlowControlEdge edge, BlockVertex vertex)
          instrumentEdge Call this to add a Vertex in place of an edge.
 

Uses of ControlFlowGraph in junit.quilt.cover.none
 

Methods in junit.quilt.cover.none with parameters of type ControlFlowGraph
 void NoneClassLoader.instrumentMethod(InstContext context, ControlFlowGraph graph)
           
 

Uses of ControlFlowGraph in junit.quilt.cover.state
 

Methods in junit.quilt.cover.state with parameters of type ControlFlowGraph
 void SMClassLoader.instrumentMethod(InstContext context, ControlFlowGraph cfg)
           
 



Copyright © 2001-2002 David Dixon-Peugh. All Rights Reserved.