1 /***
2 * ReturnEdge
3 *
4 * This is an edge which returns from
5 * the method.
6 */
7
8 package junit.quilt.cover.generic;
9
10 import junit.quilt.exception.InvalidTransitionException;
11 import org.apache.bcel.generic.*;
12
13 public class ReturnEdge
14 extends FlowControlEdge
15 {
16 public ReturnEdge( BlockVertex source ) {
17 super( source, null );
18 }
19
20 public void connect( MethodGen method,
21 InstructionList il,
22 InstructionHandle source,
23 InstructionHandle target )
24 throws InvalidTransitionException
25 {
26 if (!(source.getInstruction() instanceof ReturnInstruction)) {
27 throw new InvalidTransitionException("Return Expected.");
28 }
29 // if (source.getInstruction() instanceof ReturnInstruction) {
30 // if (target instanceof FinallyVertex) {
31 // il.insert( source, new JSR( target ));
32 // } else {
33 // throw new InvalidTransitionException("Finally expected.");
34 // }
35 // } else {
36 // throw new InvalidTransitionException("Return expected.");
37 // }
38 }
39
40 public String toString() {
41 return "[R: " + getSource() + "]";
42 }
43 }
This page was automatically generated by Maven